Search found 3 matches

by nibin89
Thu Apr 11, 2013 3:40 am
Forum: Speed Control Systems
Topic: Oriental Motor EMP 400 Controller wiring
Replies: 11
Views: 104367

Re: Oriental Motor EMP 400 Controller wiring

Thank you for the valuable information. I had made the circuit i attached previously and connected to the EMP 400. I am getting the desired output (only ALM) and Input from the EMP. But there is a problem with the READY Output. Even when the EMP is solely functioning and i type 'r' in the hypertermi...
by nibin89
Wed Apr 10, 2013 7:34 pm
Forum: Speed Control Systems
Topic: Oriental Motor EMP 400 Controller wiring
Replies: 11
Views: 104367

Re: Oriental Motor EMP 400 Controller wiring

Thank you for the reply. Actually speaking, i am using a Digital Input Output card for controlling the EMP. NI 6514 to be precise. Normal direct connection to the card does not yield any output. I have attached here with the NI DIO Card Input and Output Circuitry. Please help me verify the connectio...
by nibin89
Wed Apr 10, 2013 2:09 am
Forum: Speed Control Systems
Topic: Oriental Motor EMP 400 Controller wiring
Replies: 11
Views: 104367

Oriental Motor EMP 400 Controller wiring

Please help me connect the inputs and outputs of the EMP 402 to my PLC. As far as i know, i understand that the input pins and output pins from the CN1 cannot be directly connected to the PLC (an inbetween convertion circuitry is needed). My requirement: I need a 24 V or 0 V state change from the CN...

Go to advanced search