Search found 174 matches

by om_tech_support_JS
Thu Dec 14, 2017 12:46 pm
Forum: AC Motors
Topic: VFD Compatibility with KII Series, Single-Phase, 220 /23 V AC Geared Motors
Replies: 1
Views: 11

Re: VFD Compatibility with KII Series, Single-Phase, 220 /23 V AC Geared Motors

Hi essenceindia, In regards to your post, the 5IK90KG-5H10B is not a valid USA part number. From researching this model, it looks to be a version available on the Oriental Motor Singapore website. Although they would be able to assist you better with information on that product as well as any recomm...
by om_tech_support_JS
Thu Dec 14, 2017 10:24 am
Forum: Linear & Rotary Actuators and Controls
Topic: Can the EZED2 be substituted for the discontinued EZED1?
Replies: 11
Views: 6164

Re: Can the EZED2 be substituted for the discontinued EZED1?

Hi diepnhan,

I have shared the EZED1 file with you. Do you have the interface cable that I mentioned in the previous posting?
by om_tech_support_JS
Tue Dec 12, 2017 11:44 am
Forum: AC Motors
Topic: how do I wire a 3ik15rgn-aul w/3gn9k gearhead
Replies: 1
Views: 39

Re: how do I wire a 3ik15rgn-aul w/3gn9k gearhead

Hi Steve, In regards to your post, you can reference the bottom of page A-172 or the top of page A-173 (depending on if you are looking at doing a uni-directional or bi-directional connection) of the following link [electronically pages 3 and 4]: http://www.orientalmotor.com/products/pdfs/2000-2001/...
by om_tech_support_JS
Thu Dec 07, 2017 8:45 am
Forum: Stepper Motors and Controls
Topic: Stepper Motor Sizing
Replies: 7
Views: 188

Re: Stepper Motor Sizing

Hi Engr. Wasiu, In regards to your post, I do apologize as the value shown in the example is the incorrect value. As you stated, using the inch measurement for the desired resolution and the mili meter measurement for the pitch would result in conflicting units. With that being said, the inch units ...
by om_tech_support_JS
Fri Dec 01, 2017 3:55 pm
Forum: Stepper Motors and Controls
Topic: Stepper Motor Sizing
Replies: 7
Views: 188

Re: Stepper Motor Sizing

Hi Engr. Wasiu, The total length of the ball screw will only include the screw, therefore, you do not need to include the coupling or bearing. For the linear guide, it provides two functions. The first function is to provide an anti-rotation mechanism and the second is to handle a specific amount of...
by om_tech_support_JS
Fri Dec 01, 2017 3:12 pm
Forum: Stepper Motors and Controls
Topic: Stepper Motor with Driver combination clarification
Replies: 5
Views: 154

Re: Stepper Motor with Driver combination clarification

Hi essenceindia, In regards to your post, is the speed in degrees/second or revolutions / minute? When sending the information, is it in one of these settings, or are you sending the frequency value? Below is the speed-torque curve of the motor: https://catalog.orientalmotor.com/Asset/stc-pkp264u20_...
by om_tech_support_JS
Fri Dec 01, 2017 10:40 am
Forum: Stepper Motors and Controls
Topic: CVK Series Stepper Motor Clarifications
Replies: 1
Views: 55

Re: CVK Series Stepper Motor Clarifications

Hi essenceindia, As stated in the following post: http://forum.orientalmotor.com/viewtopic.php?f=18&t=13933 The LCS04SD5 and LC5N10 B would be the compatible cables (motor cable is now different) for the CVK544BK package. No additional accessories are required. All aspects of controlling the CVK...
by om_tech_support_JS
Fri Dec 01, 2017 10:31 am
Forum: Stepping Motors & Controls
Topic: CVK Series Controlling with PC
Replies: 7
Views: 242

Re: CVK Series Controlling with PC

Hi essenceindia, I apologize for the delay in this response. In regards to your post, the CVK525BK package consists of the PKP525N12B [Motor] and the CVD512-K [Driver]. The CVK544BK package would instead consist of the PKP544N18B [Motor] and the CVD518-K [Driver]. The two drivers will share the same...
by om_tech_support_JS
Wed Nov 22, 2017 1:14 pm
Forum: Stepper Motors and Controls
Topic: Stepper Motor with Driver combination clarification
Replies: 5
Views: 154

Re: Stepper Motor with Driver combination clarification

Hi essenceindia, In regards to your post, the CVD228(BR)-K driver would have the most optimized performance as it was originally tested with the PKP264 frame size motors. However, since your motor only requires 2.0 A/phase, then the CVD223-K driver could also be used with this motor as the maximum o...
by om_tech_support_JS
Wed Nov 22, 2017 8:51 am
Forum: Stepper Motors and Controls
Topic: Stepper Motor with Driver combination clarification
Replies: 5
Views: 154

Re: Stepper Motor with Driver combination clarification

Hi essenceindia, Good Questions! Starting with the motor and driver combination, I would actually recommend going with either the CVD228-K or CVD228BR-K driver due to the size of the motor. The first being the board type driver and the second has a mounting bracket. I have linked the comparison belo...
by om_tech_support_JS
Tue Nov 21, 2017 11:53 am
Forum: Stepper Motors and Controls
Topic: Stepper Motor Sizing
Replies: 7
Views: 188

Re: Stepper Motor Sizing

Hi Engr. Wasiu, In regards to your post, I have the following definitions: Desired Resolution (feed per pulse) : This sets the desired smallest motion for your application. It determines the linear amount (inches or mm) that the system will move based on one pulse (or step) of the motor. Feed : This...
by om_tech_support_JS
Tue Nov 21, 2017 11:40 am
Forum: Speed Control Systems
Topic: ES01 Failure
Replies: 5
Views: 181

Re: ES01 Failure

Hi rydogdav,

Have you received the RMA email? If so, please proceed with the form if you have not done so already.
by om_tech_support_JS
Tue Nov 21, 2017 7:49 am
Forum: Speed Control Systems
Topic: ES01 Failure
Replies: 5
Views: 181

Re: ES01 Failure

Hi rydogdav, Please check your email for receipt of the RMA process. In the mean time, is there any issue with the fuse in your connection? Since the speed controller has no built-in fuse for overcurrent protection, the manual instructs to install a device for overcurrent protection (e.g. fuse) befo...
by om_tech_support_JS
Mon Nov 20, 2017 9:47 am
Forum: Speed Control Systems
Topic: ES01 Failure
Replies: 5
Views: 181

Re: ES01 Failure

Hi rydogdav, In regards to your post, I apologize that you have not received a response, however, I was unfortunately unable to locate an original request sent in. Did you originally contact via phone or email? Based on your description and the application, I would advise looking at the wiring of th...
by om_tech_support_JS
Mon Nov 20, 2017 9:04 am
Forum: Stepping Motors & Controls
Topic: CVK Series Controlling with PC
Replies: 7
Views: 242

Re: CVK Series Controlling with PC

Hi essenceindia, In regards to your post, since the CVK525BK package is a connector type package, I would recommend also getting the LCS04SD5 Driver Lead Wire Set (sold as an accessory) so that you would not need to make the motor, I/O, or Power cables that connect to the driver. We also offer the L...
by om_tech_support_JS
Mon Nov 20, 2017 8:42 am
Forum: Stepper Motors and Controls
Topic: BLE motor/driver control through Modbus
Replies: 5
Views: 159

Re: BLE motor/driver control through Modbus

Hi benjaminrigsby, In regards to your post, when you said that you have our "CC-link USB cable connected to the driver," were you referring to the CC05IF-USB ? The CC05IF-USB cable will only allow you to connect our product to the MEXE02 software, but cannot be used as the communication ca...
by om_tech_support_JS
Thu Nov 16, 2017 8:44 am
Forum: Stepping Motors & Controls
Topic: CVK Series Controlling with PC
Replies: 7
Views: 242

Re: CVK Series Controlling with PC

Hi essenceindia, In regards to your post, the CVK525BK package consists of a motor (with a double shaft) and a driver. This driver is a pulse input type driver , therefore, you will need to provide this package with pulse and direction signals from an external controller. You can reference the I/O s...
by om_tech_support_JS
Wed Nov 15, 2017 3:20 pm
Forum: Stepper Motors and Controls
Topic: AZ Series Interface Control Documentation (ICD)
Replies: 14
Views: 766

Re: AZ Series Interface Control Documentation (ICD)

Hi Saad, In regards to your post, using the 24 VDC power supplies would be our recommendation for the SCX11 controller and AZD-K driver. With that being said, each product will draw the current that it needs. Therefore, your power supply will need to have a minimum of the combined current values. Fo...
by om_tech_support_JS
Mon Nov 13, 2017 2:07 pm
Forum: Stepper Motors and Controls
Topic: BLE motor/driver control through Modbus
Replies: 5
Views: 159

Re: BLE motor/driver control through Modbus

Hi benjaminrigsby, In regards to your latest post, the value that you write to the 007Dh (125 decimal) register will be dependent on the binary code that is created from turning on the specific bits. For instance: If you want to run Speed No. 0 in the forward direction. Then you would turn on bit 3....
by om_tech_support_JS
Mon Nov 13, 2017 12:58 pm
Forum: Stepper Motors and Controls
Topic: BLE motor/driver control through Modbus
Replies: 5
Views: 159

Re: BLE motor/driver control through Modbus

Hi benjaminrigsby, In regards to your post, the Speed Registers will have upper and lower values ( 1152 for Speed No. 0 Upper and 1153 for Speed No. 0 Lower). You can store up to 16 different speeds into the series of registers (Speed No. 0 ~ Speed No. 15). However, in order to have the motor move, ...
by om_tech_support_JS
Mon Nov 13, 2017 10:24 am
Forum: Linear and Rotary Actuators and Controls
Topic: Reset current position
Replies: 1
Views: 119

Re: Reset current position

Hi UE07, In regards to your post, the most common method to avoid getting the error is to create a wrap. Another alternative would be to turn on the P-Preset input which will change the current position to the value set for the position preset value (factory setting is 0). You also mentioned that th...
by om_tech_support_JS
Wed Nov 08, 2017 3:44 pm
Forum: Stepping Motors & Controls
Topic: AZ Series: Checking the Current Position of an AZ Driver via ASG and BSG outputs
Replies: 0
Views: 276

AZ Series: Checking the Current Position of an AZ Driver via ASG and BSG outputs

Q: I am using your AZD-A driver with the SCX11 controller. I want to be able to read the current position of the AZ series motor as the system may be turned off at the end of the night and turned on to start the next day. I was told that the AZD-AD driver has a Modbus register that can be read, howe...
by om_tech_support_JS
Fri Nov 03, 2017 1:18 pm
Forum: Stepper Motors and Controls
Topic: Using CVK series driver and motor with third party controller
Replies: 3
Views: 191

Re: Using CVK series driver and motor with third party controller

Hi JeraldGor,

In regards to your post, the SCX10 is a discontinued product that has been updated to the SCX11 controller. When looking at a controller for your application, I would recommend going with the SCX11:
https://catalog.orientalmotor.com/item/ ... ller/scx11
by om_tech_support_JS
Thu Oct 26, 2017 2:41 pm
Forum: Stepping Motors & Controls
Topic: Microstepping, Accuracy, and Torque
Replies: 5
Views: 2425

Re: Microstepping, Accuracy, and Torque

Hi timoluca, In regards to your correction, the original response included the statement: " Microstepping with our step motor drivers will not decrease your motor's torque output. " The key point is that our driver is smart enough to adjust the current to keep the torque constant. In a gen...
by om_tech_support_JS
Thu Oct 26, 2017 6:48 am
Forum: Stepping Motors & Controls
Topic: Microstepping, Accuracy, and Torque
Replies: 5
Views: 2425

Re: Microstepping, Accuracy, and Torque

Hi timoluca,

In regards to your post, our driver will monitor the current on the windings. Based on the monitored current, the driver will then make an adjustment in order to optimize the torque. This function is the current correction (or compensation).

Go to advanced search