Search found 3 matches

by om_tech_support_SZ
Mon Oct 09, 2017 2:20 pm
Forum: Stepping Motors & Controls
Topic: AZ: Automatic Homing using one input when torque level is met
Replies: 0
Views: 115

AZ: Automatic Homing using one input when torque level is met

Q: I am using the AZ series with the mechanical absolute sensors to operate one part of a press fit machine that we are building right now. For my application, I would like the motor to push part A into part B and once part A is in place, I would like the motor to press 2 seconds and return home aut...
by om_tech_support_SZ
Tue May 30, 2017 1:35 pm
Forum: Question of the Day
Topic: CRD FLEX (CRK series) driver: communicating through Modbus
Replies: 0
Views: 886

CRD FLEX (CRK series) driver: communicating through Modbus

CRD FLEX (CRK series) driver: communicating through Modbus Q: I am currently using the CRD Flex type driver to drive a motor used in a camera focusing application. I would like to communicate to the driver using Modbus RTU through RS-485 communication as this motor is one of the motors in a 3-axis ...
by om_tech_support_SZ
Mon Jan 23, 2017 6:16 pm
Forum: AC Motors
Topic: Permissible inertia for Brother gearmotors
Replies: 0
Views: 690

Permissible inertia for Brother gearmotors

Q: I am considering using a Brother motor( G3F40N10-MV9AWN ) to rotate a 5-kg drum mounted vertically. The drum has a diameter of 1000mm. The speed and torque characteristics of the motor meets my application needs just fine. I am unsure if the load inertia would exceed the specifications. How do I...

Go to advanced search