Search found 2 matches

by om_tech_support_AC
Wed Sep 06, 2017 12:23 pm
Forum: Stepper Motors and Controls
Topic: AZ pulse input wiring to SCX11
Replies: 0
Views: 228

AZ pulse input wiring to SCX11

Q: Is there a wiring diagram for SCX11 to AZ pulse input type in the SCX11 manual? A: Since the AZ was released after the SCX11 there is not a wiring diagram similar to the SCX11 to AR found in the operating manual. However, below is a pin for pin connection and also a sink/source connection. The SC...
by om_tech_support_AC
Fri Jan 27, 2017 2:16 pm
Forum: Speed Control Systems
Topic: External Potentiometer resistance rating effect on BLH
Replies: 0
Views: 484

External Potentiometer resistance rating effect on BLH

Q: I am using one of your BLH series brushless DC gearmotor and driver for a parts feeder. I wish to use an external potentiometer to control the speed. I read that 20 KΩ resistor is required. Do I have to use a 20 KΩ for the external potentiometer? What happens if I use a potentiometer with a diffe...

Go to advanced search