Search found 99 matches

by omsupport1
Wed Nov 23, 2011 10:52 am
Forum: Stepper Motors and Controls
Topic: Overload error when transferring PLC prog
Replies: 4
Views: 3515

Re: Overload error when transferring PLC prog

Both of those cases could cause an overlaod alarm.

I suspect that the alarm is being caused by when the load is falling after the brake is being released. Please look at why the brake is being released
by omsupport1
Mon Nov 21, 2011 10:44 am
Forum: Stepper Motors and Controls
Topic: Overload error when transferring PLC prog
Replies: 4
Views: 3515

Re: Overload error when transferring PLC prog

Sir or Madam, I am sorry that you are having difficulty. -Can you please tell us how the PLC is interacting with the ARL system? For example, is the PLC controlling the step and direction signals and perhaps also the input for the brake control? -What do you mean by "transfer my PLC programme&q...
by omsupport1
Tue Oct 11, 2011 11:02 am
Forum: Stepper Motors and Controls
Topic: CRK Stored Program Controller Motion Creator Software
Replies: 7
Views: 33495

Re: CRK Stored Program Controller Motion Creator Software

Are the moxa card outputs RS-485?

Can you give me the moxa card part #?

What baud rate are you using?

I will look into it for you.
by omsupport1
Fri Oct 07, 2011 12:52 pm
Forum: Stepper Motors and Controls
Topic: controllers for stepper motors
Replies: 9
Views: 12705

Re: controllers for stepper motors

Galil products are very good products and they have knowledgeable support persons. You should be OK.

Good luck!
by omsupport1
Fri Oct 07, 2011 9:20 am
Forum: Stepper Motors and Controls
Topic: controllers for stepper motors
Replies: 9
Views: 12705

Re: controllers for stepper motors

I would suggest that you look at a controller from a 3rd party for your coordinated motion axes, just to be safe. I am sure that you can find something out there that will operate very similar to what was originally in the machine, including using the CAD/CAM software.
by omsupport1
Fri Oct 07, 2011 9:12 am
Forum: Stepper Motors and Controls
Topic: CRK Stored Program Controller Motion Creator Software
Replies: 7
Views: 33495

Re: CRK Stored Program Controller Motion Creator Software

cowboy, Thank you for using products form Oriental Motor! The answer to your question is quite simple. The MEXE02 software works with the CRD507-K D driver/controller that you have. The Motion Creator program that you downloaded is for a different driver/controller part #, CRD507-K P . Both products...
by omsupport1
Thu Oct 06, 2011 1:18 pm
Forum: Stepper Motors and Controls
Topic: controllers for stepper motors
Replies: 9
Views: 12705

Re: controllers for stepper motors

I would suggest that you look at the EMP402-2 dual axis controller and then either an EMP402 single axis controller or the SCX10 controller. For the two axes that need to be coordinated, how coordinated do they need to be? Do you need to be able dispense a perfect cirlce (circular interpolation) of ...
by omsupport1
Thu Oct 06, 2011 11:40 am
Forum: Stepper Motors and Controls
Topic: controllers for stepper motors
Replies: 9
Views: 12705

Re: controllers for stepper motors

dolanm, Can you please describe to me how you would like to "talk" (PC, stand alone, USB, RS232, etc) to the step motor controllers? Does the motion of these three axes need to be coordinated or not? The short answer is that all of our controllers will work with these drivers. Please look ...
by omsupport1
Thu Oct 06, 2011 8:45 am
Forum: Stepper Motors and Controls
Topic: CRD5114P
Replies: 5
Views: 4892

Re: CRD5114P

Sam,

Yes, this will work with the package that you have selected. Your controller is doing all of the hard work!
by omsupport1
Thu Sep 29, 2011 8:49 am
Forum: Stepper Motors and Controls
Topic: CRD5114P
Replies: 5
Views: 4892

Re: CRD5114P

Sam,

You are correct, this driver is meant for open loop control.

It sounds like you should be looking at a servo motor for your application. By the fact that you need to close a torque loop, this the definition of a servo motor.

Is there anything else I can help you with?

Nick
by omsupport1
Mon Sep 26, 2011 10:07 am
Forum: Stepper Motors and Controls
Topic: CRD5114P
Replies: 5
Views: 4892

Re: CRD5114P

Sam,

You are correct, it is a chopper drive.

Yes, for a fixed pulse rate of 1kHz, you will sacrifice speed for smoothness and resolution, with the smooth drive disabled.

The pulse inputs are active on the Falling edge

I hope that this answers all of your questions
by omsupport1
Wed Sep 14, 2011 9:31 am
Forum: Stepper Motors and Controls
Topic: CRK controller position feedback command?
Replies: 1
Views: 2151

Re: CRK controller position feedback command?

Tom, The Hex data that you are seeing in the background is used exclusively for between the GUI and the controller at this time. Please give me a little time to see if we can make it so that you can access that data stream directly. Please email me your contact info directly at: forum@orientalmotor....
by omsupport1
Fri Aug 19, 2011 2:47 pm
Forum: AC Motors
Topic: Right Angle Hollow Shaft Gearhead Orientation
Replies: 1
Views: 5511

Re: Right Angle Hollow Shaft Gearhead Orientation

There are no mounting orientation requirements for our gearheads.

Good luck!
by omsupport1
Thu Jun 23, 2011 8:51 am
Forum: Stepper Motors and Controls
Topic: Questions from a first time stepper motor user. (CRK series)
Replies: 3
Views: 3209

Re: Questions from a first time stepper motor user. (CRK series)

Your question has three possibilities, depending on how you want to do it. 1) If a PC or PLC with serial communication is available and will be connected to the CRK Plus, you would use the "RUN xxxx" command, where xxx is the name of the your program. Please see page 213 of the manual. 2) ...
by omsupport1
Mon Jun 20, 2011 4:51 pm
Forum: Stepper Motors and Controls
Topic: Questions from a first time stepper motor user. (CRK series)
Replies: 3
Views: 3209

Re: Questions from a first time stepper motor user. (CRK series)

phbourner, Thank you for your interest in OM products. No, the CRK series does not need to have an encoder connected to the motor or controller in order to do the repeated index move program. The encoder is only used for position verification at the end of the move, if needed. As for the USB convert...
by omsupport1
Mon Jun 13, 2011 8:57 am
Forum: Stepper Motors and Controls
Topic: Step motor 5 phase with drive
Replies: 9
Views: 5444

Re: Step motor 5 phase with drive

Good job!
by omsupport1
Tue Jun 07, 2011 10:43 am
Forum: AC Motors
Topic: 5IK90GU-ATF Wiring
Replies: 2
Views: 7431

Re: 5IK90GU-ATF Wiring

Can you check your part # of 5IK90GU-ATF for me? I show that this motor has a terminal box installed onto it, which means that there are no lead wires supplied with it. If this is true, those wires (and theie color) were supplied by whoever installed the motor. If this is the correct part # , the wi...
by omsupport1
Thu May 26, 2011 1:48 pm
Forum: Stepper Motors and Controls
Topic: SCX10 Controller - Motor Current OFF USB Communication
Replies: 2
Views: 3056

Re: SCX10 Controller - Motor Current OFF USB Communication

Bryan, The answer to your question has two parts because controlling the driver current with the SCX10 involves two steps. Step 1: The command to turn the current ON & OFF is: CURRENT 0 >>>> Turns current Off CURRENT 1 >>>> Turns current ON Step 2: This command controls the CON and COFF outputs ...
by omsupport1
Wed May 18, 2011 9:16 am
Forum: Stepper Motors and Controls
Topic: Step motor 5 phase with drive
Replies: 9
Views: 5444

Re: Step motor 5 phase with drive

Good Luck!
by omsupport1
Tue May 17, 2011 9:39 am
Forum: Stepper Motors and Controls
Topic: Step motor 5 phase with drive
Replies: 9
Views: 5444

Re: Step motor 5 phase with drive

Where are you located and where do you go to school? Perhaps we can help you out somehow.
by omsupport1
Mon May 16, 2011 11:37 am
Forum: Stepper Motors and Controls
Topic: Step motor 5 phase with drive
Replies: 9
Views: 5444

Re: Step motor 5 phase with drive

Yes, as I suspected, these motors and drivers are not compatible.

By the way, where did you get them?
by omsupport1
Sun May 15, 2011 9:21 am
Forum: Stepper Motors and Controls
Topic: Step motor 5 phase with drive
Replies: 9
Views: 5444

Re: Step motor 5 phase with drive

Can you tell us a little more about what you mean by they don't work? The motor and driver part numbers are very old and have been obsolete for approximately 15 years. Also, is the driver part number that you gave me complete? If so, the motors and drivers that you have are not compatible with each ...
by omsupport1
Tue May 10, 2011 2:26 pm
Forum: Speed Control Systems
Topic: Brushless DC motor and PLC controller
Replies: 1
Views: 6959

Re: Brushless DC motor and PLC controller

Ibraim, Thank you for choosing Oriental Motor products! Yes, we have experience with HBL products working with PLC's. Are you seeing anything at the input of the PLC from the SPEED output of the HBL? Are you supplying voltage to pin 2 of the HBL driver and grounding pin 3 of the HBL driver? Since th...
by omsupport1
Wed Apr 13, 2011 6:50 am
Forum: AC Motors
Topic: Maximum Permissible Inertia
Replies: 10
Views: 20741

Re: Maximum Permissible Inertia

Please keep us updated.
by omsupport1
Mon Apr 11, 2011 10:12 am
Forum: AC Motors
Topic: Maximum Permissible Inertia
Replies: 10
Views: 20741

Re: Maximum Permissible Inertia

Sorry about forgetting about the 10^-4 factor.

What will you try to do?

Go to advanced search