Search found 11 matches

by techsupport
Fri Feb 03, 2012 2:20 pm
Forum: Stepper Motors and Controls
Topic: ASD30 series driver
Replies: 1
Views: 2219

Re: ASD30 series driver

Rebajm, To initialize parameters back to factory default, you can use the MIPRM command to initialize parameters to their initial values. You can locate the Alpha Step Plus operation manual via the link below. If you have any further questions, feel free to contact our technical support group at tec...
by techsupport
Fri Feb 03, 2012 2:14 pm
Forum: Stepper Motors and Controls
Topic: Vexta Driver UDX5128 or UDK5128N.
Replies: 3
Views: 12476

Re: Vexta Driver UDX5128 or UDK5128N.

Patrick, The reason your motor is not functioning, I cannot be certain. The unit could be over 20 years old. However, the UDX5128 is not interchangeable with the UDX5128N. The UDX5128N uses the New Pentagon Bipolar wiring setup. The UDX5128 driver used the star bipolar setup. The UPH596H-A motor wil...
by techsupport
Thu Feb 02, 2012 8:14 am
Forum: Linear and Rotary Actuators and Controls
Topic: Immediate Motion Creator for CM, Save System Config
Replies: 2
Views: 5919

Re: Immediate Motion Creator for CM, Save System Config

Hi Michael, In order to save all of the parameters from the SCX10 to a file, you will need to go to the program editor tab. You need to look under the Duplicate Heading on the right side of the screen. In the "All Data" box, click on SCX10 => PC. This will send all of the system configurat...
by techsupport
Mon Jan 23, 2012 9:41 am
Forum: Stepper Motors and Controls
Topic: Witing for 5-phase 10 leads Vexta motor
Replies: 1
Views: 3438

Re: Witing for 5-phase 10 leads Vexta motor

Hello, The wiring of the five phase motor will also depend on the type of motor driver you are using. There are two common types, Pentagon Bipolar and Star Bipolar. You should check with the manufacturer of the drive to make sure. All of the newer Oriental Motor Vexta drives use New Pentagon Bipolar...
by techsupport
Mon Jan 23, 2012 7:47 am
Forum: Stepper Motors and Controls
Topic: Vexta AS motor wiring?
Replies: 1
Views: 4234

Re: Vexta AS motor wiring?

Hello, Unfortunately, all information on the pin out of the AS motor cable is proprietary information. Technically, any modification of this cable does void the product warranty. Since the motor has a built in resolver for feedback, any miss-wiring to this section of the motor will damage the resolv...
by techsupport
Wed Jan 20, 2010 4:45 pm
Forum: AC Motors
Topic: Motor temperature
Replies: 3
Views: 6773

Re: Motor temperature

It is not getting that hot, but it gets around 150deg F. So, it sounds like the motor is fine at this temperature. My main concern is related to some plastic components nearby. Is there anything I can do to reduce the temperature of the motor?
by techsupport
Wed Jan 20, 2010 11:38 am
Forum: AC Motors
Topic: locked rotor current
Replies: 1
Views: 4981

locked rotor current

I have a BHI62FMT-7.5RA and need to know what the full load amperage draw is? Also, can you tell me what the maximum starting current or locked rotor current is?
by techsupport
Tue Jan 19, 2010 3:14 pm
Forum: Speed Control Systems
Topic: BX series
Replies: 1
Views: 4510

BX series

What does the BX motor use for feedback to the driver?
by techsupport
Mon Jan 18, 2010 5:05 pm
Forum: AC Motors
Topic: Motor temperature
Replies: 3
Views: 6773

Motor temperature

My motor case gets very hot. Should I be concerned? Is there anything I can do to reduce the temperature?
by techsupport
Mon Jan 18, 2010 5:00 pm
Forum: Stepper Motors and Controls
Topic: CRK Software
Replies: 1
Views: 2124

CRK Software

Is there an upgrade available for the CRK Stored Program type GUI?
by techsupport
Mon Jan 18, 2010 4:59 pm
Forum: AC Motors
Topic: 5IK40GN-AWU reversible?
Replies: 1
Views: 4440

5IK40GN-AWU reversible?

I have a 5IK40GN-AWU. Is this motor reversible?

Go to advanced search