Search found 8 matches

by om_tech_support_MD
Tue Sep 17, 2019 7:09 am
Forum: Stepper Motors and Controls
Topic: Multi axis driver power supply
Replies: 0
Views: 132

Multi axis driver power supply

Question: What size power supply do I need for the multi axis driver? Main power supply The main power supply is used to power the steppers. The control power supply is used to power the control board, fan, and other circuitry. We recommend using 2 separate power supplies. One for the main power sup...
by om_tech_support_MD
Thu Sep 12, 2019 8:00 am
Forum: Stepper Motors and Controls
Topic: AZ Firmware update
Replies: 0
Views: 156

AZ Firmware update

If you get an AL45 alarm on the AZ series, it is because the driver does not recognise the motor. The AZ series is constantly evolving with new products. It is currently composed of steppers, linear actuators, rack and pinion, grippers, hollow rotary actuators, and compact linear actuators. If you w...
by om_tech_support_MD
Mon May 13, 2019 6:30 am
Forum: Speed Control Systems
Topic: BLE2 Connection cables
Replies: 0
Views: 595

BLE2 Connection cables

For the BLE2 driver, you will need a connection cable between the motor to the driver. There are 2 different types of connection cables offered with this series. A forward facing or backward facing cable. It is important to note that the direction is not interchangeable. They are offered from 0.5-20...
by om_tech_support_MD
Fri May 10, 2019 12:05 pm
Forum: Speed Control Systems
Topic: BMU connection cable types
Replies: 0
Views: 539

BMU connection cable types

For the BMU driver, you will need a connection cable between the motor to the driver. There are 2 different types of connection cables offered with this series. A forward facing or backward facing cable. It is important to note that the direction is not interchangeable. They are offered from 0.5-10 ...
by om_tech_support_MD
Tue Apr 02, 2019 1:36 pm
Forum: Stepper Motors and Controls
Topic: AR absolute battery install with RS-485 (ModBUS RTU)
Replies: 0
Views: 730

AR absolute battery install with RS-485 (ModBUS RTU)

To make the AR series absolute, you need to connect the battery to store the position. As an absolute system it will store the electrical home position even after power is removed. With an absolute system, you may not need a home or limit sensor. Without the battery, when you turn on the driver, you...
by om_tech_support_MD
Fri Mar 29, 2019 10:19 am
Forum: Stepper Motors and Controls
Topic: AR absolute battery install with OPX-2A
Replies: 0
Views: 661

AR absolute battery install with OPX-2A

To make the AR series absolute, you need to connect the battery to store the position. As an absolute system it will store the electrical home position even after power is removed. With an absolute system, you may not need a home or limit sensor. Without the battery, when you turn on the driver, you...
by om_tech_support_MD
Thu Mar 28, 2019 8:02 am
Forum: Stepper Motors and Controls
Topic: AR absolute battery install with MEXE02
Replies: 0
Views: 663

AR absolute battery install with MEXE02

To make the AR series absolute, you need to connect the battery to store the position. As an absolute system it will store the electrical home position even after power is removed. With an absolute system, you may not need a home or limit sensor. Without the battery, when you turn on the driver, you...
by om_tech_support_MD
Fri Dec 07, 2018 9:56 am
Forum: General Discussion
Topic: EtherCAT protocol CiA301 VS CiA402
Replies: 0
Views: 1233

EtherCAT protocol CiA301 VS CiA402

EtherCAT protocol CiA301 VS CiA402 Question: I want to use the AZD4A-KED multi axis driver with EtherCAT, but can’t run all 4 steppers at the same time because of the high amperage draw. Is there an alternative. Responce: The CiA CANopen embedded network is a bus system used to link multiple devices...