Search found 4 matches

by icontrolthings
Thu Sep 07, 2017 2:59 pm
Forum: Stepper Motors and Controls
Topic: A MATLAB example codes with RS485 Modbus RTU
Replies: 3
Views: 12677

Re: A MATLAB example codes with RS485 Modbus RTU

Were you ever able to properly control via matlab?
by icontrolthings
Fri Sep 01, 2017 12:02 pm
Forum: Stepper Motors and Controls
Topic: Controlling AZD-AD via Matlab
Replies: 1
Views: 279

Controlling AZD-AD via Matlab

I was wondering if it is at all possible to control the AZD-AD driver directly via Matlab (connecting to CPU via RS-485). I essentially need to be able to send a sequence of commands (move to + 180, move back to -180, go home, repeat) and read back absolute positions from the encoder, and was wonder...
by icontrolthings
Thu Aug 24, 2017 3:38 pm
Forum: Stepping Motors & Controls
Topic: AZD-A to SCX11 I/O
Replies: 3
Views: 393

Re: AZD-A to SCX11 I/O

Thanks! I am still having a slight issue however. I double checked that the wiring is correct, so let me walk you through what I did. 1. Went into IMC software, under driver I/O settings I had output 8 set as just OUT8. 2. Saved and reset 3. Wired Pin 3 of the Driver (IN4) to Pin 10 of the Controlle...
by icontrolthings
Thu Aug 24, 2017 10:52 am
Forum: Stepping Motors & Controls
Topic: AZD-A to SCX11 I/O
Replies: 3
Views: 393

AZD-A to SCX11 I/O

I am currently using the SCX11 controller to connect to the AZD-A driver. I would like to be able to execute the ZHOME command which is available in the MEXE02 software, but on the IMC Software. I have been trying to configure the I/O on both the driver and controller so that I can send a signal fro...

Go to advanced search