Introducing New MEXE02 Stored Data Editing Software v3.03

Announcements related to New Products, Trainings, Software Updates, etc can be found here.
User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Introducing New MEXE02 Stored Data Editing Software v3.03

Postby om_tech_support_JT » Tue May 13, 2014 11:57 am

Oriental Motor has made significant improvements to our MEXE02 Data Setting Software, adding more functions to common screens and offering the ability to have multiple windows open. This software is available for download via our website.

The MEXE02 software is used for our FLEX line of products (Stored Data type drivers) and NX Series servo motor packages. The software was improved to increase the user friendliness along with improved functions. Also, with the AR Series drivers now part of the DGII and EAS / EAC, the MEXE02 now easily supports those products as well.

SUMMARY OF IMPROVEMENTS:

Navigation
The header and side bar have been added to improve the user friendliness and make the functions easily visible. Now, when clicking on a topic, a new window will appear for that function.

Multi Monitor Function
Multiple screens can now be open at once allowing for example teaching and I/O monitoring to be visible at the same time.

MEXE02 v3.03 navigation, multi-monitor function.jpg
MEXE02 v3.03 navigation, multi-monitor function.jpg (118.96 KiB) Viewed 4960 times

Teaching / Remote Operation Screens: Several functions have been added to this screen to improve the control, efficiency and ease of use when using the MEXE02.

I/O Status:
Now the I/O is visible when Teaching / Remote Operation screen is open.

Reflecting on the driver:
Don’t have to be offline now to utilize setting the data points in the driver when teaching.

Soft Limit Teaching:

Easy to see and set on one screen.

MEXE02 v3.03 IO status, soft limit teaching.jpg
MEXE02 v3.03 IO status, soft limit teaching.jpg (108.14 KiB) Viewed 4960 times


Waveform Monitor
The waveform monitor screen has been updated to have all the necessary functions on the screen.

Scale Function has been added to the screen for even greater monitoring abililty.

CH and Trigger functions are now visible vs being on another screen.

Copy to clipboard was also added to this screen for ease of use.

MEXE02 v3.03 new waveform monitor functions.jpg
MEXE02 v3.03 new waveform monitor functions.jpg (124.01 KiB) Viewed 4960 times

New products have been added to the drop down menu for selection and with the AR Series drivers now part of the DGII and EAS / EAC, the MEXE02 now easily supports those products by selecting the AR Series. For AR Pulse Input type, the remote operation function has been added.

MEXE02 v3.03 other advantages.jpg
MEXE02 v3.03 other advantages.jpg (37.72 KiB) Viewed 4960 times

Summary of Applicable products: all FLEX (stored data) products
AR Series
DG II Series (via AR Series)
EAS / EAC Series (via AR Series)
CRK Series (Stored Data)
RKII Series
PKA Series
BLE Series
DG II Series
EAS / EAC Series
-and NX Series

To download the software, please visit our website => DOWNLOADS => SOFTWARE DOWNLOADS => MEXE02 Data Setting Software, v3.03:
http://www.orientalmotor.com/support/so ... tware.html

PLEASE MAKE SURE TO ALSO DOWNLOAD THE REQUIRED DRIVER FOR USB CABLE (CC05IF-USB). If you are purchasing a FLEX product, we can include 1pc free CC05IF-USB cable as part of our FLEX promotion (upon request). It will connect our FLEX driver to your PC's USB COM port in order to use the MEXE02 software.

Return to “Latest Announcements”

Who is online

Users browsing this forum: No registered users and 1 guest