AR series push motion/current setting driver update

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

AR series push motion/current setting driver update*

Postby om_tech_support_JT » Tue Sep 01, 2015 7:20 pm

Q: I have an ARD-A stepper motor driver which I am trying to set up Push Motion operation to 60% using the MEXE02 v3.12 data edit software. However, every time I perform a data-write operation to the driver, the following errors are generated.

AR series push motion setting driver update - error 1A57F038.jpg
AR series push motion setting driver update - error 1A57F038.jpg (32.03 KiB) Viewed 2366 times

After pressing OK I received the following error.

AR series push motion setting driver update - error 1A57F038.jpg
AR series push motion setting driver update - error 1A57F038.jpg (32.03 KiB) Viewed 2366 times

What can I do to resolve this error?

A: Since January 6, 2014, there has been an update to the AR series drivers. There are differences in data setting range, etc. between the product after the change and before the change. For the driver before the specification change, contact your nearest Oriental Motor sales office. These changes include the following:
1. Some setting items have been changed
• Push current specifications changed from 0 to 500 (1=0.1%) to 0 to 1000 (1=0.1%)
• NET-IN input function
i. 24: ALM-RST
ii. 25: P-PRESET
iii. 26: P-CLR
NOTE: When the data is set using the MEXE02, use the MEXE02 software version is 3.00 or later

2. The upper limit of the alarm output has been changed
• Maximum speed for push-motion operation changed from 30rpm to 500rpm
For more information regarding this change please reference page 6-7 of the manual below
http://www.orientalmotor.com/products/p ... 065-7E.pdf

If you have a driver purchased before January 6, 2014 please contact Oriental Motor Technical Support at 1-800-468-3982 for assistance.

LR

aldoned
Posts: 32
Joined: Mon Sep 14, 2015 3:03 am

Re: AR series push motion/current setting driver update

Postby aldoned » Fri Apr 22, 2016 4:11 am

Thanks for the info


Return to “Stepping Motors & Controls”

Who is online

Users browsing this forum: No registered users and 2 guests