ARD-CD Driver and Arm66mc-ps25

heru
Posts: 2
Joined: Mon Sep 21, 2015 11:31 pm

ARD-CD Driver and Arm66mc-ps25

Postby heru » Mon Sep 21, 2015 11:43 pm

Dear Admin and All,

I just buy ARD-CD Driver and Arm66mc-ps25. Is it possible to control ARD-CD with plc via CN9 and CN8? please share


Thanks

heru
Posts: 2
Joined: Mon Sep 21, 2015 11:31 pm

Re: ARD-CD Driver and Arm66mc-ps25

Postby heru » Tue Sep 22, 2015 1:09 am

Hi,

From another discussion at this forum, I get some step how to control I/O with plc directly.
1. setting parameter with MEXE02 or the OPX-2A.
2. read the output at cn9 and write the input at cn8.

Is it correct? please share

thanks

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: ARD-CD Driver and Arm66mc-ps25

Postby om_tech_support_JT » Wed Sep 30, 2015 1:56 pm

Hi heru,

I think this post would be most helpful in explaining how to program and execute motion with our stored data products such as the AR66MCD-PS25-3 package model which you are using.

viewtopic.php?f=26&t=716&sid=848

I have also attached a Flex brochure which explains all capabilities of stored data / Flex products.

FLEX_web_Brochure.pdf
(589.55 KiB) Downloaded 129 times

There are several methods to program/control the AR66MCD-PS25-3 motor+driver with built-in stored data controller. The easiest method would be to use the MEXE02 software to set all your data and parameters, then use PLC to execute with I/O. You do need the CC05IF-USB cable to connect the ARD-CD driver to your PC in order to communicate with the MEXE02 software.

Please let us know if you would like me to explain anything in more detail.

crossby
Posts: 3
Joined: Fri Oct 28, 2016 2:18 am

Re: ARD-CD Driver and Arm66mc-ps25

Postby crossby » Fri Oct 28, 2016 2:20 am

Thank for help


Return to “Stepping Motors & Controls”

Who is online

Users browsing this forum: No registered users and 2 guests