change new model from PH264M-32 to PK264AM

knightstinger
Posts: 1
Joined: Fri Aug 12, 2011 1:06 am

change new model from PH264M-32 to PK264AM

Postby knightstinger » Fri Aug 12, 2011 1:20 am

Q: before this i use stepping motor model PH264M-32,due to this model discontinued,so i change to PK264AM.but the problem is,when i connect this PK264AM to the existing controller,the motor speed cannot get low rpm.the lowest speed PK264AM achieve is 41rpm but i need the speed can go down until 10rpm.is it i can use the old driver which is use at PH264M-32?tq

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: change new model from PH264M-32 to PK264AM

Postby om_tech_support_JT » Mon Aug 15, 2011 3:40 pm

Hi knightstinger,

Before I can answer your question, I need to confirm the replacement motor part number in order to do a comparison. We do not manufacture a PK264AM motor. I would also need information on your driver/amplifier such as the brand/model, voltage on the power supply, and current output. Information on your machine/motor setup would be helpful as well as any other changes you might have done to the machine (pulleys, sprockets, ball screw....etc.).


Return to “Stepping Motors & Controls”

Who is online

Users browsing this forum: No registered users and 2 guests