EZS II Series & Alphastep Plus Driver: Exceeding Max Speed

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

EZS II Series & Alphastep Plus Driver: Exceeding Max Speed

Postby om_tech_support_JT » Wed Jan 05, 2011 6:56 pm

Q: If I am using your Alphastep Plus driver with built-in programmable pulse generator to control your EZS II series linear slide (which allows a faster speed to be set). Can I run the linear slide faster than its rated speed?

A: We do not recommend doing so as the specifications (such as accuracy, torque, and life) will differ if operated outside of the linear slider product's designed specifications. The slider may also exhibit erratic behavior and excessive noise at beyond the maximum rated speed since the ball screw in the slider was not designed for operation beyond the maximum rated speed. Warranty will also be voided. If you need a faster speed, please ask about our SPV series of belt-driven actuator systems, or the EZX series ball screw actuator systems.

paulwalker_92
Posts: 10
Joined: Sun Jul 10, 2011 5:12 am

Re: EZS II Series & Alphastep Plus Driver: Exceeding Max Speed

Postby paulwalker_92 » Sun Jul 10, 2011 5:33 am

Thanks for the support :)

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: EZS II Series & Alphastep Plus Driver: Exceeding Max Speed

Postby om_tech_support_JT » Fri Jul 22, 2011 3:46 pm

You're welcome Paul. If you have any interesting topics that you would like us to explain more in detail, please let me know.


Return to “Linear & Rotary Actuators and Controls”

Who is online

Users browsing this forum: No registered users and 1 guest