Moment Loads: Definitions and Calculations

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Moment Loads: Definitions and Calculations

Postby om_tech_support_JT » Wed Apr 04, 2012 5:27 pm

Q: What are moment loads?

A: We show specific maximum moment loads allowable for our linear actuators in our literature. Each actuator has a specific maximum pitch moment, yaw moment, and roll moment loads. If these values are exceeded, then we cannot guarantee the longevity of the components inside our actuators, and expected life of the actuator will be reduced.

SEE PAGE E-30 (TOP-RIGHT CORNER):
http://www.orientalmotor.com/products/p ... o_ezs2.pdf

Page E-30 shows that the EZS4D025-C model can handle a 8 Nm of dynamic (moving) pitch moment load, and a 51.2 Nm of static (resting) pitch moment load. This means that it can move a 10 N off-centered load where the center of gravity of the load is 5.12 meters away from the center of the carriage of the actuator (vertical direction).

SEE PAGE G-19 FOR DEFINITIONS OF PITCH/YAWING/ROLLING MOMENTS:
http://www.orientalmotor.com/products/p ... lation.pdf

If you were using our mounting brackets, then we would have a maximum load and stroke for each XY or XZ configuration with moment loads already calculated.

SEE PAGE E-105:
http://www.orientalmotor.com/products/p ... n_acce.pdf

For example, if you used an EZS4D for X-axis, and an EZS3D for Y-axis, and the X actuator is carrying the Y actuator, then the maximum load on the Y actuator is 2.3 kg or less, and the stroke is limited to 300 mm on the Y-axis.

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Moment Loads: Definitions and Calculations

Postby om_tech_support_JT » Fri May 04, 2012 3:55 pm

SUPPLEMENT INFORMATION: TYPES OF MOMENT LOADS EXPLAINED GRAPHICALLY

Moment Loads.jpg
Moment Loads.jpg (280.94 KiB) Viewed 4863 times


For more details, please see the PAGE G-19 LINK in the previous post.


Return to “Linear & Rotary Actuators and Controls”

Who is online

Users browsing this forum: No registered users and 1 guest