ARD-CD driver data setting via rs485 Communication

mhar101
Posts: 2
Joined: Wed Sep 30, 2015 8:11 pm

ARD-CD driver data setting via rs485 Communication

Postby mhar101 » Wed Sep 30, 2015 8:25 pm

Hi our company purchased a EACM4D20ARMC linear actuator with ARD-CD, AR Series Driver with Built-in Controller (Stored Data) (Single-Phase 200-240 VAC), we dont have neither the OPX-2A nor the CC05IF-USB cable, the last option is setting the data via RS485 Communication, can you give us a tutorial on how to do this setting, what hardware we be using as well as the software.

thank you we will appreciate if you answer this.

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: ARD-CD driver data setting via rs485 Communication

Postby om_tech_support_JT » Mon Oct 26, 2015 6:16 pm

Hi mhar101,

To be able to set the stored data within the ARD-CD driver via RS-485, you need to have a working knowledge of Modbus RTU open source industrial communication protocol which is derived from master/slave architecture. You also need your own software either included with the PLC you're using, or developed on your own.

The only tutorial we have is something like this:
viewtopic.php?f=26&t=716

Here's some general info about Modbus:
https://en.wikipedia.org/wiki/Modbus

If you do not have your own software, you can download a freeware like this (however, it's only offered as a test software):
ComTest Pro: http://www.baseblock.com/PAGES/ACDRIVES/BEE.htm

However, if you do not have working knowledge of Modbus RTU protocol, it could take a while to learn.

I would highly suggest that you download the MEXE02 software from here to make your job easier and quicker:
http://www.orientalmotor.com/support/so ... tware.html

And request the CC05IF-USB cable for free from your local Oriental Motor office here:
http://www.orientalmotor.com/company/locator.epl
or
http://www.orientalmotor.com/company/gl ... pport.html

The MEXE02 software includes several helpful functions such as I/O monitor, I/O assignments, I/O logic, motor parameters and more. These functions have proved very useful during the initial setup/test phase. It's also much easier and quicker to use for setting data as well as internal motor/driver parameters. In the USA, we typically have the cable in stock so we can ship same day.

artmuz62
Posts: 10
Joined: Wed Dec 14, 2016 4:58 am

Re: ARD-CD driver data setting via rs485 Communication

Postby artmuz62 » Wed Dec 14, 2016 5:01 am

Thank you for the advice guys! I also encountered this problem) It worked!


Return to “General”

Who is online

Users browsing this forum: No registered users and 3 guests