When to use PK564AW

Discuss Stepper motors, Drivers, Controllers, GUI's and related Accessories here.
dongxam626
Posts: 5
Joined: Mon Oct 21, 2013 8:18 pm

When to use PK564AW

Postby dongxam626 » Wed Oct 23, 2013 6:16 pm

Hi
Please What is the major different between PK564AW and PK564AUA.

Thank You

dongxam626
Posts: 5
Joined: Mon Oct 21, 2013 8:18 pm

Re: When to use PK569AW

Postby dongxam626 » Wed Oct 23, 2013 6:18 pm

I am sory , The question is What is the major different between PK569AW and PK569AUA.

Thank You

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: When to use PK564AW

Postby om_tech_support_JT » Thu Oct 24, 2013 11:11 am

Both of these motors are older US standard products but they are still available. The PK596AW model can still ship same day, but not the PK569AUA model.

By the way, the dedicated driver for the PK569AUA motor is the DFR1514A driver (115VAC). The dedicated driver for the PK569AW motor is the RKD514L-A (115VAC) or RKD514L-C (230VAC, single-phase).

Both motors are rated for 1.4 A/ph current. Both the DFR1514A and RKD514L-A/C will provide up to 1.4 A/ph max. Both are the same frame size and stack length. The PK569AW motor has a 8 mm shaft diameter while the PK569AUA has a 5/16" mm shaft diameter.

Here are the links to these specific motor and driver combination packages:

RK SERIES (PK569AW + RKD514L-A = RK569AA PACKAGE)
WEB: http://catalog.orientalmotor.com/item/a ... cy/rk569aa
SUGGESTED REPLACEMENT: http://catalog.orientalmotor.com/item/a ... s/rk569aae

RFK SERIES (PK569AUA + DFR1514A = RFK569AA PACKAGE)
WEB: http://catalog.orientalmotor.com/item/a ... s/rfk569aa
SUGGESTED REPLACEMENT: http://catalog.orientalmotor.com/item/p ... s/crk569ap

The RK569AA or its replacement package, RK569AAE, uses AC power so it can output more high speed torque than the RFK569AA or its replacement package, CRK569AP (which only uses 24VDC power).

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: When to use PK564AW

Postby om_tech_support_JT » Thu Oct 24, 2013 11:13 am

By the way, the RKD514L-A is a newer 115VAC version of the UDK5114x driver you were requesting information for.

artmuz62
Posts: 10
Joined: Wed Dec 14, 2016 4:58 am

Re: When to use PK564AW

Postby artmuz62 » Wed Dec 14, 2016 6:21 am

Unfortunately, I do not know how to use! (
Children have told, I think they are right!


Return to “Stepper Motors and Controls”

Who is online

Users browsing this forum: No registered users and 1 guest