function of M0 M1 M2 in RKSD503-CD

Discuss Stepper motors, Drivers, Controllers, GUI's and related Accessories here.
RISKIFITRAYADI
Posts: 2
Joined: Mon Aug 21, 2017 8:08 pm

function of M0 M1 M2 in RKSD503-CD

Postby RISKIFITRAYADI » Mon Aug 21, 2017 8:12 pm

HELLO,

i want asking about driver stepper type RKSD503-CD, what is function M0 M1 and M2 in control input?

thanks

riski

om_tech_support_JS
Posts: 175
Joined: Tue May 10, 2016 4:48 pm

Re: function of M0 M1 M2 in RKSD503-CD

Postby om_tech_support_JS » Tue Aug 22, 2017 12:45 pm

Hi Riski,

In regards to your post, the RKSD503-CD driver is a built-in controller (Stored Data) type driver. Therefore, you can store up to 64 different data points to this driver which you can then operate via the I/O. The M0 to M5 inputs can be used in a binary configuration in order to select the operation data number. Once the operation data number is selected, then the START input can be triggered and the operation can be run. Below is a reference to the binary configuration table for the M0 to M5 inputs. This table can be found on page 49 of the manual:
http://www.orientalmotor.com/products/p ... 085-4E.pdf

M0 to M5 inputs.png
M0 to M5 inputs.png (382.8 KiB) Viewed 264 times

RISKIFITRAYADI
Posts: 2
Joined: Mon Aug 21, 2017 8:08 pm

Re: function of M0 M1 M2 in RKSD503-CD

Postby RISKIFITRAYADI » Wed Aug 23, 2017 1:49 am

Ok thank you for the information


Return to “Stepper Motors and Controls”

Who is online

Users browsing this forum: No registered users and 1 guest