AZ pulse input wiring to SCX11

Discuss Stepper motors, Drivers, Controllers, GUI's and related Accessories here.
om_tech_support_AC
Posts: 2
Joined: Tue Jan 03, 2017 2:53 pm

AZ pulse input wiring to SCX11

Postby om_tech_support_AC » Wed Sep 06, 2017 12:23 pm

Q: Is there a wiring diagram for SCX11 to AZ pulse input type in the SCX11 manual?

A: Since the AZ was released after the SCX11 there is not a wiring diagram similar to the SCX11 to AR found in the operating manual. However, below is a pin for pin connection and also a sink/source connection. The SCX11 must sink or source with 24 VDC, the 5 VDC does not provide enough voltage for the AZ pulse input. For the SCX11 all the inputs and outputs can be assigned using our immediate motion creator software which can be downloaded for free using the link below or a terminal software. The AZ pulse input type uses our free to download MEXE02, also linked below to assign the input and outputs. Please note the first 4 inputs are used for the pulse inputs.

Software Download

SCX11 Wiring.JPG
SCX11 Wiring.JPG (111.64 KiB) Viewed 45 times

Return to “Stepper Motors and Controls”

Who is online

Users browsing this forum: No registered users and 1 guest