I need help, I am working at a science museum and I am making an exhibit that contains a 60" stroboscopic disc. With a motor I need to spin the 50 pound disk anywhere from 30 to 500 rpm. With a potentiometer I would like to gradually change the rpm in very small steps around 1 rpm in resolution. It is also important that motor maintain the set rpm precisely and not wander. I have to run it from 120V AC power 700-watt max. I am told that I need an inverter drive and an AC brushless motor to achieve this. Can anyone recommend a motor and drive system for less than $1000?
Many thanks,
Steve.