Motor temperature

Discuss AC Induction motors, Reversible motors, Synchronous motors, Low-Speed Synchronous motors, Torque motors, Gearheads, Brake Packs and related Accessories here.

Motor temperature

Postby techsupport » Mon Jan 18, 2010 4:05 pm

My motor case gets very hot. Should I be concerned? Is there anything I can do to reduce the temperature?
User avatar
techsupport
 
Posts: 6
Joined: Tue Jan 05, 2010 7:59 am

Re: Motor temperature

Postby omsupport1 » Wed Jan 20, 2010 11:21 am

How hot is hot?

Based on the winding insulation class that Oriental Motor uses, the motor case temperature should not exceed 90°C (194°F).

Is you motor hotter than this?
Oriental Motor Product Forum Support
forum@orientalmotor.com
User avatar
omsupport1
 
Posts: 30
Joined: Thu Nov 19, 2009 9:34 am

Re: Motor temperature

Postby techsupport » Wed Jan 20, 2010 3:45 pm

It is not getting that hot, but it gets around 150deg F. So, it sounds like the motor is fine at this temperature. My main concern is related to some plastic components nearby. Is there anything I can do to reduce the temperature of the motor?
User avatar
techsupport
 
Posts: 6
Joined: Tue Jan 05, 2010 7:59 am

Re: Motor temperature

Postby omsupport1 » Wed Jan 20, 2010 3:53 pm

I don't know if any of these options will be appropriate for you, but you could try:
-Reducing the duty cycle of the motor's "ON" or "running" time
-If the motor is in an enclosure, make sure that there air can flow through the enclosure
-Use a fan to force air across or around the motor.

Are the plastic parts being affected by the motor temperature of 150°F? I would think that plastic would have much higher melting point that 150°F.
Oriental Motor Product Forum Support
forum@orientalmotor.com
User avatar
omsupport1
 
Posts: 30
Joined: Thu Nov 19, 2009 9:34 am


Return to AC Motors

Who is online

Users browsing this forum: No registered users and 1 guest

cron