Oriental AC Motors with VFD Combination Suitablity

Discuss AC Induction motors, Reversible motors, Synchronous motors, Low-Speed Synchronous motors, Torque motors, Gearheads, Brake Packs and related Accessories here.
Post Reply
essenceindia
Posts: 34
Joined: Thu Nov 16, 2017 7:46 am

Oriental AC Motors with VFD Combination Suitablity

Post by essenceindia » Mon Apr 16, 2018 3:53 am

Hi !!

Good Day !!

Please let us know whether Oriental Three-Phase, (220~415 V AC) motors would be comparable with any of third party VFD combination for variable speed controlling ??

Also whether Single-Phase, 220~230 V AC motors would be possible to varying the speed / frequency with third party VFD ??

Please let us know your valued feedback to enable us to proceed further in this regard.

thanking you & best regards,

Shree

om_tech_support_AC
Posts: 46
Joined: Tue Jan 03, 2017 2:53 pm

Re: Oriental AC Motors with VFD Combination Suitablity

Post by om_tech_support_AC » Mon Apr 16, 2018 1:38 pm

Hi Shree,

All the three phase induction motors on the website are VFD rated. You can use them with a third-party VFD or we can recommend a Fuji Inverter based on the motors power (W or HP) and input voltage VAC.

For the single phase 220~230 VAC induction motors those are not VFD rated. However we offer Brushless DC motors with single phase VAC input that offer provide speed control.

Bryant
Posts: 1
Joined: Tue Jun 05, 2018 3:00 am

Re: Oriental AC Motors with VFD Combination Suitablity

Post by Bryant » Tue Jun 12, 2018 4:50 am

Are there alternatives to the Fuji Inverter by the way? I'm just curious.

om_tech_support_AC
Posts: 46
Joined: Tue Jan 03, 2017 2:53 pm

Re: Oriental AC Motors with VFD Combination Suitablity

Post by om_tech_support_AC » Tue Jun 12, 2018 6:41 am

Hi Bryant,

Oriental Motor only offers Fuji inverters. If you would like a Third-party inverter can be used with our three phase induction motors.

Post Reply