5IK90GU-ATF Wiring

Discuss AC Induction motors, Reversible motors, Synchronous motors, Low-Speed Synchronous motors, Torque motors, Gearheads, Brake Packs and related Accessories here.
radman
Posts: 1
Joined: Wed Jun 01, 2011 4:58 pm

5IK90GU-ATF Wiring

Postby radman » Wed Jun 01, 2011 5:03 pm

I have a 5IK90GU-ATF motor. The motor has 4 wiring terminals.
1)White
2)Yellow?
3)Blue
4)A gray or purple?

What is the correct method to wire this motor?

User avatar
omsupport1
Posts: 99
Joined: Thu Nov 19, 2009 10:34 am

Re: 5IK90GU-ATF Wiring

Postby omsupport1 » Tue Jun 07, 2011 10:43 am

Can you check your part # of 5IK90GU-ATF for me? I show that this motor has a terminal box installed onto it, which means that there are no lead wires supplied with it. If this is true, those wires (and theie color) were supplied by whoever installed the motor.

If this is the correct part # , the wiring would be like this:

For CW rotation:
Terminal 1 >> One side of the capacitor
Terminal 2 >> To one of the power supply legs and the other side of the capacitor
Terminal 3 >> To the other leg of the power supply
Terminal 4 >> Jumpered to terminal 3

For CCW rotation:
Terminal 1 >> Jumpered to terminal 3
Terminal 2 >> To one of the power supply legs and one side of the capacitor
Terminal 3 >> To the other leg of the power supply
Terminal 4 >> To other side of the capacitor


Let me know if this helps!
Oriental Motor Product Forum Support
forum@orientalmotor.com

paulwalker_92
Posts: 10
Joined: Sun Jul 10, 2011 5:12 am

Re: 5IK90GU-ATF Wiring

Postby paulwalker_92 » Sun Jul 10, 2011 5:18 am

Thanks for your support. It is nice knowledge for me too.


Return to “AC Motors”

Who is online

Users browsing this forum: No registered users and 2 guests