5Ik40 Wireing

Discuss AC Induction motors, Reversible motors, Synchronous motors, Low-Speed Synchronous motors, Torque motors, Gearheads, Brake Packs and related Accessories here.
hawkseye
Posts: 2
Joined: Sat Feb 04, 2012 7:07 pm

5Ik40 Wireing

Postby hawkseye » Sat Feb 04, 2012 7:10 pm

Someone know the wireing in english... 110 v single... 2 post cap... I have lead wires white , blue, black, yellow
This is an induction motor, 100V .8A 10uf

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: 5Ik40 Wireing

Postby om_tech_support_JT » Mon Feb 06, 2012 11:54 am

I assume the full part number is 5IK40GN(or A)-A from the description of 5IK40 motor with AC100 v input, 10 micro farad capacitor, and lead wire colors black, blue, yellow and white.
If this is correct, the wiring is following. (There is no English manual for this motor since it was not made for the USA environment.)
For CW rotation, tie Black and Blue together and connect to AC (L), connect Yellow and AC (N) to one side of capacitor terminals, and connect White to the other side of the capacitor terminals.
For CCW rotation, tie Yellow and Blue together and connect to AC(L), connect Yellow and AC(N) to one side of capacitor terminals, and connect Black to the other side of the capacitor terminals.
Please keep in mind, the motor is only rated for AC 100v. Connecting AC 110v is not recommended.
I will recommend using a transformer to lower the voltage or using 5IK40GN-AW2U that is rated for AC110v and AC115v.

hawkseye
Posts: 2
Joined: Sat Feb 04, 2012 7:07 pm

Re: 5Ik40 Wireing

Postby hawkseye » Wed Feb 08, 2012 5:30 am

Yes it is, I seemed to have forgot the A.... Thanks for the info.!

reeja
Posts: 1
Joined: Wed Dec 24, 2014 3:28 am

Re: 5Ik40 Wireing

Postby reeja » Wed Dec 24, 2014 3:32 am

Thanks for this great info :D :D :D
Get free demos for E20-517 braindumps exam and mcts exam with Test king guaranteed success. Our best quality usuhs prepares you well before appearing in the final exams of www.bgsp.edu and mcts with Quincy University

rey234
Posts: 1
Joined: Wed Feb 10, 2016 4:12 am

Re: 5Ik40 Wireing

Postby rey234 » Wed Feb 10, 2016 4:16 am

Hi There, Thanks for the link, but I also tried GOOGLE. And other sites.. I saw a lot of diagram from internet, the OM site it self, BUT I never saw a diagram describing the output I have. BLUE, BLACK, YELLOW, WHITE... The one, you send also describe about it, BUT the WIRE Color are, RED, WHITE, BLUE. Only 3-color wire. The other connection with BLUE/WHITE/BLACK is for 3-phase, but as the Model itself suggest single phase (5IK40GN-"A").

Pass4sure 350-080
Pass4sure VCAP5-DCD Dumps
Pass4sure 70-409 Exam

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: 5Ik40 Wireing

Postby om_tech_support_JT » Tue Feb 23, 2016 5:52 pm

Hi rey234,

If I understand you correctly, the description I gave on this post previously does describe a 4-wire motor with the colors you mentioned.

For CW rotation, tie Black and Blue together and connect to AC (L), connect Yellow and AC (N) to one side of capacitor terminals, and connect White to the other side of the capacitor terminals.

For CCW rotation, tie Yellow and Blue together and connect to AC(L), connect Yellow and AC(N) to one side of capacitor terminals, and connect Black to the other side of the capacitor terminals.

Magdalena
Posts: 1
Joined: Thu Jul 14, 2016 12:02 am

Re: 5Ik40 Wireing

Postby Magdalena » Thu Jul 14, 2016 12:12 am

I kinda do it, the only thing I need is the connection where to put what color on what connection. I seen some model but the colors are different, this is why I don't want to connect it without checking the standard coloring for this Model. I don't have the electrical diagram so even if I will get electricial it the same thing he will ask me first

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: 5Ik40 Wireing

Postby om_tech_support_JT » Thu Jul 14, 2016 10:02 am

Please see the general wiring diagrams below for 4 wire AC motors such as the 5IK40A-A or 5IK40GN-A. It also includes some wiring info for 3 wire motors. If you have a specific part number for the motor, please provide it. We offer many motors in different parts of the world and the wiring could be different.

4 & 3-wire AC motor wiring diagrams.jpg
4 & 3-wire AC motor wiring diagrams.jpg (131.54 KiB) Viewed 10364 times


Return to “AC Motors”

Who is online

Users browsing this forum: No registered users and 1 guest