Helical pinion

Discuss AC Induction motors, Reversible motors, Synchronous motors, Low-Speed Synchronous motors, Torque motors, Gearheads, Brake Packs and related Accessories here.
Post Reply
ratonxi
Posts: 1
Joined: Thu Apr 05, 2012 3:17 am

Helical pinion

Post by ratonxi » Thu Apr 05, 2012 3:20 am

hi there,

I am the proud owner of a 2GN90K gearhead. The problem is that i want to use this gearHead with a Brushless motor, not the single phase AC motor. I would need some information on the helical pinion gear that I would need to use my BL motor in order to use it with this gearhead. Could you provide a store where I can purchase the helical pinion? Or do you know the info of the pinion gear that I would need?

Thank you in advance

User avatar
om_tech_support_JT
Posts: 1057
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Helical pinion

Post by om_tech_support_JT » Thu Apr 05, 2012 8:43 am

The 2GN90K gearhead was designed mainly for AC motors and it's an older version. Our new RoHS compliant gearheads feature twice the expected life and quieter operation (2GN90S for 8mm shaft dia; 2GN90SA for 5/16" shaft dia). We have one older brushless motor system that still uses the 2GN type gearheads, which is our AXU series. Please see recommended model number below:

[ AXU210A-GN ]
WEB: http://catalog.orientalmotor.com/item/a ... xu210a-gnx
-fits any 2GN type gearhead.
-1.1~22 RPM, 26 lb-in continuous, constant torque output.

We do not sell just the helical pinion shaft or gears. We also do not show our pinion shaft in our literature because our gearheads were designed only to work with our motors, and we sell them as a packaged product.

Here are the rest of our brushless round-shaft and gearmotor systems:
http://www.orientalmotor.com/products/b ... index.html

Let me know if you have any more questions.

Post Reply