Request for correct wiring diagram for 5RK40GK-AA 115V 60hz

Discuss AC Induction motors, Reversible motors, Synchronous motors, Low-Speed Synchronous motors, Torque motors, Gearheads, Brake Packs and related Accessories here.
wchill09
Posts: 1
Joined: Thu Apr 25, 2013 10:38 pm

Request for correct wiring diagram for 5RK40GK-AA 115V 60hz

Postby wchill09 » Thu Apr 25, 2013 10:42 pm

Could someone please help me find the correct wiring diagram for a 5RK40GK-AA 40W 115v 60hz motor? Also, is this a capacitor type motor and if so, what value should I use. Many thanks in advance for this help.
Bill

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Request for correct wiring diagram for 5RK40GK-AA 115V 60hz

Postby om_tech_support_JT » Fri Apr 26, 2013 1:40 pm

Hi Bill,

Please see below for the specifications and wiring diagram of your 5RK40GK-AA motor. The wiring method and specifications are the same as a 5RK40A-AA motor which is shown below:

5RK40A-AA, 5RK40GK-AA motor wiring diagram, specifications.jpg
5RK40A-AA, 5RK40GK-AA motor wiring diagram, specifications.jpg (127.73 KiB) Viewed 5129 times

The specifications also state that the motor requires a 12.0 microfarad/250VAC rated capacitor.


Return to “AC Motors”

Who is online

Users browsing this forum: No registered users and 1 guest