How to find the Maximum frequency output from a PIC

Discuss anything that may not be product related here.
Barlioh
Posts: 4
Joined: Sun Sep 11, 2016 10:59 pm

How to find the Maximum frequency output from a PIC

Postby Barlioh » Mon Sep 19, 2016 8:27 pm

I used to watch a thread was dealing with maximum frequency output from a PIC for any given master clock. Unfortunately my searches did not return any good information.

I’m interested to get a small PIC device (10F or 12F type)to act as a high frequency clock generator using its internal clock and I wouldlike to know what to expect.
I have an application where the space is very tight and Ineed a modulated clock source with decent stability in the order of hundreds ofkHz but ideal will be 1MHz.
Manufacturer Part#:
PIC12F675-I/MF
Product Category: Embedded - Microcontrollers
Manufacturer: Microchip Technology
Description: IC MCU 8BIT 1.75KB FLASH 8DFNS
PIC12F675-I/MF Datasheet
Package: 8-VDFN Exposed Pad
Quantity: 1030 PCS
Lead Free Status / RoHS Status: Lead free / RoHS Compliant
Moisture Sensitivity Level(MSL): 3(168 Hours)
Using PBP I understand that something like:

main_loop:
Togglepin_x
GOTOmain_loop

should give maximum frequency output. Assuming that theToggle and GOTO commands will take two cycles each that will give me possibleoutput frequency of Main_clock/4/4 which will be 250 kHz for a 4MHz clock.
My question is if one uses Assembly (which is not my strongestfield) will it get any faster? Will itbe possible to make it run in the background?
Ideally I need a 1 MHz output that will be ON for 15 mS andOFF for 5 mS.

Thank you in advance for any advice.

om_tech_support_JS
Posts: 164
Joined: Tue May 10, 2016 4:48 pm

Re: How to find the Maximum frequency output from a PIC

Postby om_tech_support_JS » Wed Sep 21, 2016 7:26 am

Hi Barlioh,

The PIC12F675-I/MF which you are referencing is not manufactured by Oriental Motor. Therefore, you will need to contact the manufacturer of the PIC12F675-I/MF (Microchip Technology) to get further assistance with the maximum frequency. If you are interested in the maximum frequency that one of our drivers can handle, then I would require the Oriental Motor driver part number.


Return to “General Discussion”

Who is online

Users browsing this forum: Google [Bot], Perep1963 and 4 guests