Hello im looking for this motor

Discuss anything that may not be product related here.
jose juan
Posts: 1
Joined: Wed Sep 28, 2016 2:07 pm

Hello im looking for this motor

Postby jose juan » Wed Sep 28, 2016 2:18 pm

Hi Guys, im looking for this motor or something similar. I have no experience with motor or specs so i was wondering if someone could help me find it.

Image



In the label it says Induction Motor
25N 110v 60Hz 0.46A 6.5 F 1450
25N 115v 60Hz 0.46A 6.5 F 1450
Ins. Class A(51)

Thats what i can see in the label.

om_tech_support_JS
Posts: 166
Joined: Tue May 10, 2016 4:48 pm

Re: Hello im looking for this motor

Postby om_tech_support_JS » Mon Oct 03, 2016 11:39 am

Jose juan,

Unfortunately I was unable to see the image of the label which you have attached. From the description that you provided, it is most likely another manufacturer's motor as our typical motor insulation class rating is Class B and not A.

Our induction motors have a proprietary pinion style shaft which will mate with one of our gearheads (if applicable). Therefore, can you please provide me with the information on your current gearhead (if applicable)?


When we cross another manufacturer's motor to one of our motors, the speed, torque, and inertia characteristics are compared to ensure that the replacement motor will work in your existing application. However, if you are unable to obtain the specifications of the old motor, then do you know what the speed, torque, and inertia requirements are for your application?


Return to “General Discussion”

Who is online

Users browsing this forum: No registered users and 3 guests