Specify external torque in sizing tool

Discuss anything that may not be product related here.
ammaratef45
Posts: 1
Joined: Tue Oct 25, 2016 8:40 pm

Specify external torque in sizing tool

Postby ammaratef45 » Tue Oct 25, 2016 8:44 pm

I wanted to use sizing tool to choose DC motor that can handle my system, http://www.orientalmotor.com/support/ballLeadScrew.html

I didn't understand what is required in the external force? what is different between it and load?

om_tech_support_JS
Posts: 166
Joined: Tue May 10, 2016 4:48 pm

Re: Specify external torque in sizing tool

Postby om_tech_support_JS » Wed Oct 26, 2016 2:08 pm

Hi ammaratef45,

When sizing the application, both the load and external force will be needed to do a proper sizing. When sizing for a ball/lead screw, the manufacturer of the screw may have an external force that is specified for their screw. Otherwise, the external force can be seen as any force, or resistance, that is preventing the motion of the load. If there is no external force specified by the manufacturer of the ball/lead screw, or if there is no additional force, then you can use a value of 0 for the external force section.


Return to “General Discussion”

Who is online

Users browsing this forum: No registered users and 3 guests