Alpha Stepper and Drive

Discuss anything that may not be product related here.
gregouellette
Posts: 3
Joined: Tue Mar 14, 2017 5:00 pm

Alpha Stepper and Drive

Postby gregouellette » Wed Mar 15, 2017 4:14 am

I am rebuilding a Powerarm CNC router. this thing is a beast weighs over 1500 lbs.. I am a newbie to this but I understand it
ASD16D-C AlphaStep Closed-Loop Drive and a VEXTA ASM69AC steppers on the Z axis, this replaced the Mitsubishi servo motor and drive.
with the ASM911AC stepper and ASD20A-C drive on the X and Y axis. My issue now is I need to find a breakout board and a smoothstepper so I can use Mach 3.
It is using a 3 hp Portercable route but I want to upgrade to a VFD in the near future.

Any help and input would be greatly appreciated.

om_tech_support_JS
Posts: 166
Joined: Tue May 10, 2016 4:48 pm

Re: Alpha Stepper and Drive

Postby om_tech_support_JS » Wed Mar 15, 2017 8:11 am

Hi gregouellette,

Please reference the original forum post which includes pictures of the application:
viewtopic.php?f=3&t=4693&p=8703#p8703


Return to “General Discussion”

Who is online

Users browsing this forum: Yahoo [Bot] and 2 guests