BLE2 Connection cables

Discuss Brushless DC Motor Speed Control Systems or AC Motor Speed Control systems and related Accessories here.
Post Reply
om_tech_support_MD
Posts: 6
Joined: Wed Dec 05, 2018 1:49 pm

BLE2 Connection cables

Post by om_tech_support_MD » Mon May 13, 2019 6:30 am

For the BLE2 driver, you will need a connection cable between the motor to the driver. There are 2 different types of connection cables offered with this series. A forward facing or backward facing cable. It is important to note that the direction is not interchangeable. They are offered from 0.5-20 meters in length.
BLM connection cable.png
BLM connection cable.png (80.71 KiB) Viewed 23 times

The B type connector faces away from the output shaft noted in the picture below.
backwards type (B type).png
backwards type (B type).png (154.71 KiB) Viewed 23 times

The F type connector faces towards the output shaft noted the picture below. If you have a round shaft (a motor without a gearbox attached to the motor), the F type cable will not be able to bend enough if there is something above the motor mount. With a gear box, the added space would allow the cable to flex enough to bend out of the way. If you need the F type connection on a motor that does not have a gearbox, you would need to make sure nothing is impeding the cable where it is mounted.
forwards type (F type).png
forwards type (F type).png (157.58 KiB) Viewed 23 times

In addition to the connection cable, we also offer a flexible cable and an extension cable. The flexible and extension cables will go in between the connection cable and the driver. The maximum total length of the cables can not exceed 20.5 meters to prevent electrical noise.
viewtopic.php?f=23&t=17411&p=22062&hili ... end#p22062
BLE2 connection, flexible, and extersion cable.png
BLE2 connection, flexible, and extersion cable.png (56.81 KiB) Viewed 23 times

The connection cable is connected to CN4, CN2, and the ground on the driver. Be sure to fully seat the connection cable on the motor before locking the lever.
BLE2 installing cable.png
BLE2 installing cable.png (163.15 KiB) Viewed 23 times

Should you have any further questions please contact us at techsupport@orientalmotor.com or call at 1-800-GO VEXTA.

Post Reply