BXS460C-A-3, Brushless DC Motor Speed Control System

Discuss Brushless DC Motor Speed Control Systems or AC Motor Speed Control systems and related Accessories here.
cbbeh
Posts: 1
Joined: Tue Apr 25, 2017 4:58 am

BXS460C-A-3, Brushless DC Motor Speed Control System

Postby cbbeh » Wed May 10, 2017 5:15 pm

Hi,

Looking for O-Motor for my Turntable (Record Player) project, please recommend
Purchase BXS460C-A-3, Brushless DC Motor too bad it's very noisy :?

Thanks
Best regards

om_tech_support_JS
Posts: 172
Joined: Tue May 10, 2016 4:48 pm

Re: BXS460C-A-3, Brushless DC Motor Speed Control System

Postby om_tech_support_JS » Fri May 12, 2017 7:28 am

Hi cbbeh

In regards to your question, we manufacture various motor products which are typically used in industrial applications. In these types of applications, the noise specification is not a main consideration for the application. Furthermore, the noise generated may be dependent on the speed, load, and gearing of the motor. For these reasons, the dB rating of our motor products is not shown. Since this value is not shown, it would be difficult to compare your current BXS460C-A-3 system to one that would be quieter.

For further information on how the motor speed and gearing affects the noise generated, you can also reference this Forum post:
viewtopic.php?f=23&t=561&p=824&hilit=noise+rating#p824


For my reference, why was the BXS460C-A-3 package originally chosen? Do you control the speed of the table, or is the speed set and you are looking for a good value of speed regulation?


Return to “Speed Control Systems”

Who is online

Users browsing this forum: No registered users and 1 guest