Holding Torque

Discuss Brushless DC Motor Speed Control Systems or AC Motor Speed Control systems and related Accessories here.
ax20
Posts: 9
Joined: Wed Jan 04, 2017 12:41 am

Holding Torque

Postby ax20 » Tue Jul 18, 2017 3:12 am

OM,

I have a question about all BLH motors that doesn't come with brake.

What is the mechanism/force that holds the motor in place when current is on, with no rotation (0 rpm), but it seems hard to rotate the shaft.

No electromagnetic brake, no other mechanical brake? Can I know the holding force derived from catalog?

Many thanks.

om_tech_support_JS
Posts: 149
Joined: Tue May 10, 2016 4:48 pm

Re: Holding Torque

Postby om_tech_support_JS » Tue Jul 18, 2017 7:06 am

Hi ax20,

Is there a part number in particular that you are currently using from the BLH series? The BLH series does not have a holding torque value. Holding torque is generated from a stepper motor, however the BLH series is part of our Brushless DC Speed Control packages. From the speed-torque curve of the BLH series, there is no reference to a specific amount of torque at 0 RPM:

BLH Series Speed-Torque Curves.png
BLH Series Speed-Torque Curves.png (147.61 KiB) Viewed 151 times


Is there a gearhead that is being used with the motor? If so, the gearing will create a resistance when attempting to rotate by hand. This resistance is a product of the mechanical gearing and is not designed for specification. Therefore, there is no value of holding torque specified for the BLH series.


Return to “Speed Control Systems”

Who is online

Users browsing this forum: No registered users and 2 guests