Need manuals for BLD224-S

Discuss Brushless DC Motor Speed Control Systems or AC Motor Speed Control systems and related Accessories here.
wmayhugh
Posts: 2
Joined: Tue Oct 08, 2013 10:35 am

Need manuals for BLD224-S

Postby wmayhugh » Tue Oct 08, 2013 10:43 am

Anyone have the manuals for a BLD224-S Brushless Motor Speed Control Driver and a BL315GK-24S Motor? Both are Vexta products. I have been all over the internet with no luck.

The main reason I need the manual is so I can hook up the external pot. I am hooking it up per the picture on the top of the controller, but I don't have any speed control. Nor do I have any speed control with the on board speed control pot. Also, if I don't install an external pot the motor won't run.

User avatar
om_tech_support_JT
Posts: 1055
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Need manuals for BLD224-S

Postby om_tech_support_JT » Wed Oct 09, 2013 6:34 pm

Hi wmayhugh,

Please see attached for the BLS series brushless motor/driver datasheet which includes the information you need. See page 2 for information on external potentiometer, internal potentiometer, and external analog voltage. All 3 can be used to set the speed of your motor.

For external potentiometer, you would wire your 20 Kohm, 1/4W potentiometer's 3 terminals to driver screw terminals 5, 6, and 7. Both the START/STOP, RUN/BRAKE inputs need to be ON in order for the motor to rotate.

Please let me know if you have any questions.
Attachments
BLS English.pdf
(478.21 KiB) Downloaded 594 times

wmayhugh
Posts: 2
Joined: Tue Oct 08, 2013 10:35 am

Re: Need manuals for BLD224-S

Postby wmayhugh » Sun Oct 13, 2013 10:37 am

Thanks for the docs and the information. I'm a little embarrassed :oops: to say that the 2 motor units I have had crimped brown wires which caused the motor to ignor the speed control. Once I fixed that, everything worked correctily. The info for the onboard speed control was worth the wait.

waleed444
Posts: 1
Joined: Sun Feb 22, 2015 10:21 pm

Re: Need manuals for BLD224-S

Postby waleed444 » Sun Feb 22, 2015 10:31 pm

For external potentiometer, you would wire your 20 Kohm, 1/4W potentiometer's 3 terminals to driver screw terminals 5, 6, and 7. Both the START/STOP, RUN/BRAKE inputs need to be ON in order for the motor to rotate.
Our Actual Exams and Testking ccna certification gre exam provide you 100% pass comptia certification You can get access to quincy toefl and with Miami International University of Art & Design resources of http://www.selftestengine.com/.


Return to “Speed Control Systems”

Who is online

Users browsing this forum: No registered users and 1 guest