Force of 60kg on a static Rotary Actuator DG2 series

Discuss Linear or Rotary Actuators, GUI's and related Accessories here.
jasonthoe
Posts: 6
Joined: Wed Dec 08, 2010 9:14 pm

Force of 60kg on a static Rotary Actuator DG2 series

Postby jasonthoe » Tue Jun 23, 2015 6:43 pm

Could you please advise if DG130R-ARMC-3 could withstand a load of 60kg acting on the static actuator which held by the electromagnetic brake that is mounted on a flat platform .

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Force of 60kg on a static Rotary Actuator DG2 series

Postby om_tech_support_JT » Wed Jun 24, 2015 9:24 am

Hi jasonthoe,

I'm having problems visualizing how exactly the 60 kg force is acting on the DG130R-ARMC-3 rotary actuator. In our literature, we show permissible torque, holding torque at motor standstill, holding torque by electromagnetic brake, moment load, thrust/axial load specifications and even table deflection by moment load. Can you elaborate? Is the force acting upon the actuator while it's at standstill/not moving? How far away is the force from the center of the rotation axis?

Most of the specifications or links for more info can be found on this page:
http://catalog.orientalmotor.com/item/a ... 30r-armc-3


Return to “Linear and Rotary Actuators and Controls”

Who is online

Users browsing this forum: No registered users and 1 guest