Stepper motor selection for rack and pinion system

Discuss Linear or Rotary Actuators, GUI's and related Accessories here.
rahulmon
Posts: 1
Joined: Sun Apr 12, 2015 10:23 pm

Stepper motor selection for rack and pinion system

Postby rahulmon » Sun Apr 12, 2015 10:51 pm

Hi,
I would like to design a system in which a stepper motor can drive a hollow column of length 30 inch, diameter 2 inch weight 5kg in vertical direction (up and down) about 4 inches using rack and pinion system in a velocity of 1cm/s. There will be an inclination of 15 degree from the horizontal angle. How to select an appropriate motor to drive such a system.r. How to calculate the power and out put torque needed for the motor. Will the size of the motor will be very high? Is it possible to reduce the torque needed by including gear system?

Thanks ,
Rahul

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Stepper motor selection for rack and pinion system

Postby om_tech_support_JT » Mon May 11, 2015 6:04 pm

Hi rahulmon,

We ask that you try to complete the Rack & Pinion application form on this page:
http://www.orientalmotor.com/support/motor-sizing.html
and complete the positioning motion profile. We would recommend that you select a motor with an electromagnetic brake in order to prevent the load from sliding downward on the 15 deg inclination when the power is turned off. When a stepper motor is not powered, it cannot provide holding torque.

The form will calculate your required torque, load inertia, and speed. Once you have these numbers and provide a list of application requirements, we can help you select an ideal product from our vast product lineup. If you need help during sizing, one of our technical support engineers would be happy to help you through the process. We can be reached at 800-468-3982.


Return to “Linear and Rotary Actuators and Controls”

Who is online

Users browsing this forum: No registered users and 1 guest