Oriental Motor EMP 400 Controller wiring

Discuss Brushless DC Motor Speed Control Systems or AC Motor Speed Control systems and related Accessories here.
nibin89
Posts: 3
Joined: Wed Apr 10, 2013 2:01 am

Oriental Motor EMP 400 Controller wiring

Postby nibin89 » Wed Apr 10, 2013 2:09 am

Please help me connect the inputs and outputs of the EMP 402 to my PLC.

As far as i know, i understand that the input pins and output pins from the CN1 cannot be directly connected to the PLC (an inbetween convertion circuitry is needed).

My requirement:
I need a 24 V or 0 V state change from the CN1 pins ALM and READY. (EMP Outputs)
Also how can i connect my PNP sensors to the IN1, IN2, M0, M1, START pins of the EMP CN1. (EMP Inputs)

Please help.

Thank you in advance.

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Oriental Motor EMP 400 Controller wiring

Postby om_tech_support_JT » Wed Apr 10, 2013 6:46 pm

Hi,

Many of our products are designed to be controlled with a PLC; including the EMP series controllers. Please see the following wiring diagram for the CN1 connector on the EMP controller (scroll down to view entire diagram; inputs on top/outputs at bottom):

EMP CN1 connector wiring diagram to PLC, host controller.jpg
EMP CN1 connector wiring diagram to PLC, host controller.jpg (134.14 KiB) Viewed 105026 times

Your PLC would be the "host controller etc." on the left. There's only one way to wire the EMP controller, so just follow the wiring diagram.

The EMP outputs are open-collector types so you'll actually have to supply 5 to 24VDC to our outputs from your PLC's input. All our output circuit does is open and close the transistor to GND. If no voltage is supplied from the PLC side, then no voltage will be output when the output turns on/closes. You'll need PNP output transistors on your PLC's input side since we're sinking on our side.

You will also see from the wiring diagram above that you can only use NPN transistors with our CN1 inputs.

Here's the link to the EMP series operating manual: http://www.orientalmotor.com/products/p ... 036-3E.pdf

Our newest controller, SCX11, offers both sink/source as well as 5v/24v I/O capabilities and a GUI software. It may work for you, but it's only designed to control one motor/driver at a time. The EMP402 model is a dual-axis controller. For more information on any of our product models, please do a part number search on our main website.

Let me know if you have any questions.

nibin89
Posts: 3
Joined: Wed Apr 10, 2013 2:01 am

Re: Oriental Motor EMP 400 Controller wiring

Postby nibin89 » Wed Apr 10, 2013 7:34 pm

Thank you for the reply.

Actually speaking, i am using a Digital Input Output card for controlling the EMP. NI 6514 to be precise.
Normal direct connection to the card does not yield any output.

I have attached here with the NI DIO Card Input and Output Circuitry.
Please help me verify the connection diagrams for the EMP inputs and Outputs attached.

Thank you in advance.
Attachments
EMP to NI 6514.pdf
Connection Circuitry
(69.66 KiB) Downloaded 7655 times

nibin89
Posts: 3
Joined: Wed Apr 10, 2013 2:01 am

Re: Oriental Motor EMP 400 Controller wiring

Postby nibin89 » Thu Apr 11, 2013 3:40 am

Thank you for the valuable information.

I had made the circuit i attached previously and connected to the EMP 400.
I am getting the desired output (only ALM) and Input from the EMP.

But there is a problem with the READY Output.
Even when the EMP is solely functioning and i type 'r' in the hyperterminal, i always get READY = 0.

The READY output is always zero and never am i getting a 1 in the hyperterminal. (even after 3 sec after power on, as said in the manual)

Please help.

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Oriental Motor EMP 400 Controller wiring

Postby om_tech_support_JT » Thu Apr 11, 2013 11:38 am

The READY output will only turn on when a program is not already executing or being modified. Do you have a program named "99" or "CONFIG"? Type "EDIT" and then ENTER to get into your program directory to see if that program exists. Program "99" automatically executes upon power-up or RESET command. Either delete that program or change the name to something else. You can also tell if a program is already running by simply trying to run another program. If a program is already running, it cannot execute another program. It will give you an error message. Press the ESCAPE key to immediately exit the program.

If the READY output bit never changes to "1" or on in the R status report, then we may have a damaged output circuit. The ALM and READY outputs wire to the EMP in exactly the same way.

Do you have any alarms? What type? Do you have the E-STOP input wired to -COM?

aldoned
Posts: 32
Joined: Mon Sep 14, 2015 3:03 am

Re: Oriental Motor EMP 400 Controller wiring

Postby aldoned » Thu Sep 17, 2015 11:56 pm

I need a 24 V or 0 V state change from the CN1 pins ALM and READY.

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Oriental Motor EMP 400 Controller wiring

Postby om_tech_support_JT » Wed Sep 30, 2015 1:18 pm

Hi aldoned,

With the EMP series controller, only the ALM output NO/NC logic can be changed with the ACTL command.

Please see PAGE 63 of the manual for more info:
http://www.orientalmotor.com/products/p ... 036-3E.pdf

library55
Posts: 1
Joined: Tue Jul 05, 2016 6:55 am

Re: Oriental Motor EMP 400 Controller wiring

Postby library55 » Mon Aug 15, 2016 8:11 am

Thank you for the info

crossby
Posts: 3
Joined: Fri Oct 28, 2016 2:18 am

Re: Oriental Motor EMP 400 Controller wiring

Postby crossby » Fri Oct 28, 2016 2:21 am

Great in formation

kong664852
Posts: 3
Joined: Tue Nov 22, 2016 11:28 pm

Re: Oriental Motor EMP 400 Controller wiring

Postby kong664852 » Tue Nov 22, 2016 11:30 pm

Thanks for the info

ong1599623
Posts: 3
Joined: Wed Nov 23, 2016 1:23 am

Re: Oriental Motor EMP 400 Controller wiring

Postby ong1599623 » Wed Nov 23, 2016 1:24 am

:lol:

ms500
Posts: 3
Joined: Tue Dec 20, 2016 9:24 pm

Re: Oriental Motor EMP 400 Controller wiring

Postby ms500 » Tue Dec 20, 2016 11:19 pm

It great!!! Thanks for the info


Return to “Speed Control Systems”

Who is online

Users browsing this forum: No registered users and 1 guest