Blow air in or vent air out?

Discuss AC or DC Axial Fans, Centrifugal Blowers, Cross Flow Fans, Thermostats and related Accessories here.
njohantgen
Posts: 6
Joined: Thu Nov 19, 2009 4:49 pm

Blow air in or vent air out?

Postby njohantgen » Mon Dec 07, 2009 2:27 pm

Which method is more effective for cooling an enclosure, blowing air into the enclosure or venting (sucking) air out of the enclosure?

User avatar
omsupport1
Posts: 99
Joined: Thu Nov 19, 2009 10:34 am

Re: Blow air in or vent air out?

Postby omsupport1 » Mon Dec 07, 2009 4:11 pm

The main points to consider when using a fan for ventilation and cooling are:
-The airflow path should be as uninterrupted as possible. Air should flow over/under the item(s) to be cooled. The air should not be forced to try to flow through the item(s) to be cooled.
-Make sure that the air flow path is not so short that it allows any air elsewhere in the enclosure to remain stagnant.

If the above conditions are met, there is no real fundamental (theoretical) difference between blowing air in or venting air out. However, in the real world, venting air out is more effective at maintaining stable internal enclosure temperature.
Oriental Motor Product Forum Support
forum@orientalmotor.com

sanamgulzar
Posts: 1
Joined: Wed Jan 21, 2015 12:16 am

Re: Blow air in or vent air out?

Postby sanamgulzar » Wed Jan 21, 2015 12:17 am

This is very nice and cool post thanks for this .........!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
sunny

kong664852
Posts: 3
Joined: Tue Nov 22, 2016 11:28 pm

Re: Blow air in or vent air out?

Postby kong664852 » Tue Nov 22, 2016 11:29 pm

Thanks for the info

ong1599623
Posts: 3
Joined: Wed Nov 23, 2016 1:23 am

Re: Blow air in or vent air out?

Postby ong1599623 » Wed Nov 23, 2016 1:25 am

Thanks to a very low

ms500
Posts: 3
Joined: Tue Dec 20, 2016 9:24 pm

Re: Blow air in or vent air out?

Postby ms500 » Tue Dec 20, 2016 9:26 pm

It great!!! Thanks for the info


Return to “Thermal Management”

Who is online

Users browsing this forum: No registered users and 0 guests