Communicate with an AZD-KD step driver using a laptop

Discuss Linear or Rotary Actuators, GUI's and related Accessories here.
Post Reply
jcacace
Posts: 1
Joined: Sun Jun 03, 2018 11:33 pm

Communicate with an AZD-KD step driver using a laptop

Post by jcacace » Mon Jun 04, 2018 12:06 am

Hi to all,

I am really new of modbus and step motor controllers like the AZD-KD, so sorry for my (hopefully) simple questions. I bought a solution with 3 AZD-KD connected via RJ45 connectors. For what I understand I have 1 master and 2 slaves. On the last slaves a RJ45 connector is free. I want to know if is possible to control all the motors using such port. I tried to search for a RJ45 -> USB adapter, but I am not sure that this will be enough to implement the modbus protocol in RTU mode.

Can you give me some hints to start the communication?? I have tried to connect my laptop using the mini-usb port on the side of the controller, and I am able to get/set parameters and position, but I want to implement a control loop for all the motors of my system

Thank you!

om_tech_support_AC
Posts: 46
Joined: Tue Jan 03, 2017 2:53 pm

Re: Communicate with an AZD-KD step driver using a laptop

Post by om_tech_support_AC » Mon Jun 04, 2018 7:07 am

Hi Jcacace,

For the USB to RS485 converter it would be suggested to use the MWE820A. For more information about MWE820A and the pinouts please refer to the document below.

http://www.orientalmotor.com/products/p ... )-v2-0.pdf

It is possible to control up to 31 slaves using a master controller over RS-485. The mini-usb port on the AZD-KD only allows for communication with a single driver via a PC. Linked below is the start of Modbus RTU/RS-485 setup, wiring and communication examples for the AZ series.

http://www.orientalmotor.com/products/p ... f#page=260

Aro
Posts: 6
Joined: Thu Aug 09, 2018 5:52 am

Re: Communicate with an AZD-KD step driver using a laptop

Post by Aro » Thu Aug 09, 2018 6:09 am

Hi everybody,

I am working too with the AZD-KD and I have no experience in Modbus RTU. I d'like to know how do I connect the RS485 cable to a laptop? In the doc, it is indicated that a commercially available LAN cable can also be used to connect the driver, does it mean an Ethernet RJ 45 cable ?

om_tech_support_AC
Posts: 46
Joined: Tue Jan 03, 2017 2:53 pm

Re: Communicate with an AZD-KD step driver using a laptop

Post by om_tech_support_AC » Thu Aug 09, 2018 6:53 am

Hi Aro,

With the MWE820A you can convert the RS485 communication or RJ45 connection into a USB connection for a laptop. For more information please refer to the link below.

https://www.orientalmotor.com/products/ ... B_v1_0.pdf

Aro
Posts: 6
Joined: Thu Aug 09, 2018 5:52 am

Re: Communicate with an AZD-KD step driver using a laptop

Post by Aro » Thu Aug 09, 2018 8:02 am

Thanks a lot,

I was not thinking of cutting the other extremity of a RJ45 cable. Now it is more clear in my mind.

Post Reply