DG200R-ARACD2-1 - Direction

Discuss Linear or Rotary Actuators, GUI's and related Accessories here.
Post Reply
jaypee4528
Posts: 2
Joined: Fri Jul 27, 2018 2:58 am

DG200R-ARACD2-1 - Direction

Post by jaypee4528 » Fri Jul 27, 2018 3:37 am

Hello

I am using a DG200R-ARACD2-1 which i control via Modbus TCP using a communicator. This means that I am unable to send a negative step-signal to the motor. So at the moment, all positions are given as a positiv, and results in CCW rotation.

I was hoping to solve my problem by changing the parametre "Motor Rotation direction". But with "Positive Direction=CCW" and with "Positive Direction=CW" the result of a positive stepcommand is always CCW.

Any ideas?

Best Regards Jes Peter

om_tech_support_AC
Posts: 46
Joined: Tue Jan 03, 2017 2:53 pm

Re: DG200R-ARACD2-1 - Direction

Post by om_tech_support_AC » Fri Jul 27, 2018 8:22 am

Hi Jes Peter,

When you changed the Motor Rotation direction did you change it using the MEXE02 software or by writing to register 0385h? When you send a move command over Modbus are you doing absolute movements or incremental?

jaypee4528
Posts: 2
Joined: Fri Jul 27, 2018 2:58 am

Re: DG200R-ARACD2-1 - Direction

Post by jaypee4528 » Thu Aug 02, 2018 2:19 am

Hello

I have changed the Parametre via Modbus and the register 0385h.

I have tried both both inc and abs, both result in CCW move with the same step command.

Best Regards Jes Peter

om_tech_support_AC
Posts: 46
Joined: Tue Jan 03, 2017 2:53 pm

Re: DG200R-ARACD2-1 - Direction

Post by om_tech_support_AC » Thu Aug 02, 2018 8:21 am

Once you wrote 0 to register 0385h you have to save the parameter change to the non-volatile memory. The register for the non-volatile memory is 0191h where you write a 1 to save the change. When you complete the writing to the non-volatile memory cycle the power of the driver.

Post Reply