Fuji multi speed

Discuss Brushless DC Motor Speed Control Systems or AC Motor Speed Control systems and related Accessories here.
Post Reply
om_tech_support_KR
Posts: 32
Joined: Thu Jan 11, 2018 3:03 pm

Fuji multi speed

Post by om_tech_support_KR » Fri Mar 29, 2019 7:54 am

Q: I want to set 2 speeds on the Fuji inverter that I’m using on a conveyor.

A: First you will need to change the F01 function code from 4 to 7 to read speed set in the I/O terminals instead of the pot.
F1.png
F1.png (100.07 KiB) Viewed 186 times
Then you will need to set your speeds in Hz by inputting them in the C05 and C06 function codes. You can set up to 15 different speed with the C05-C19 function codes.
F2.png
F2.png (40.23 KiB) Viewed 186 times
Next to change the inputs on the I/O you will have to change some of the E function codes. You will need to change the E02 (X2) function code to 1 (SS2) the factory setting is 7 (Coast to a stop). The E01 (X1) function code already has 0 (SS1) factory set. If you need to use all 15 speeds you can use the E03 (X3), E98 (FWD) or E99 (REV) function codes.
F3.png
F3.png (104.82 KiB) Viewed 186 times
F4.png
F4.png (96.48 KiB) Viewed 186 times
When SS1 is ON it will run speed set in C05 parameter and when SS2 is on it will run the speed set in the C06 parameter. Reference the table below for the speed selection.
F6.png
F6.png (39.61 KiB) Viewed 186 times
Below are some wiring examples you can wire in sink or source and use the internal voltage or external 24 VDC.
F8.png
F8.png (119.54 KiB) Viewed 186 times
F9.png
F9.png (181.49 KiB) Viewed 186 times
F7.png
F7.png (94.35 KiB) Viewed 186 times
Should you have any further questions please contact us at techsupport@orientalmotor.com or call at 1-800-GO VEXTA.

Post Reply