LAS Series, Rack and Pinion System

Discuss Linear or Rotary Actuators, GUI's and related Accessories here.
Post Reply
Mr.Thota
Posts: 25
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

LAS Series, Rack and Pinion System

Post by Mr.Thota » Fri May 31, 2019 7:04 am

Hi,
We have recently purchased LAM4F40AW-1 + LSD20A-W for moving forward direction only.

The function of the drive is up on signal the stepper motor moved forward, at the same time there will be load applied in load cell. After reaching of set load in load cell, the load cell will give signal to the drive for stop the stepper drive. After holding of set time the servo drive supposed to be comes back to original condition. But in this case the stepper motor is moving forward direction only.

There is no alaram signal from driver, requesed to please let us know the exact proble to identify and resolve the same.

Requesting you to please suggest us to rectify the drive problem.

om_tech_support_KR
Posts: 62
Joined: Thu Jan 11, 2018 3:03 pm

Re: LAS Series, Rack and Pinion System

Post by om_tech_support_KR » Fri May 31, 2019 11:34 am

Hi Mr.Thota,

Since this is a pulse input type driver first you would have to check the driver and controller are both set to same pulse input mode. If both are using the same pulse mode 1 pulse or 2 pulse mode then you can check the wiring is correct. I will link the manual for your reference.

HL-8024E.pdf
(595.41 KiB) Downloaded 62 times

Post Reply