Torque Setting & Limit Feedback

Discuss Stepper motors, Drivers, Controllers, GUI's and related Accessories here.
Post Reply
Mr.Thota
Posts: 23
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Torque Setting & Limit Feedback

Post by Mr.Thota » Thu Jun 13, 2019 5:45 am

Hi !!

As we are looking for 0 to 500 rpm minimum, Torque 2Nm and Torque feedback to be required.
Ex: toruq should not be exceeding above 2 NM, when torque reaches 2 Nm and we require feedback signal from the motor.

Pls consider motor should control through PLC output.

Requested to please suggest us best suitable motor along with technical details to proceed further.

thanks in advance.

Regards,

om_tech_support_KR
Posts: 58
Joined: Thu Jan 11, 2018 3:03 pm

Re: Torque Setting & Limit Feedback

Post by om_tech_support_KR » Thu Jun 13, 2019 10:26 am

Hi Mr.Thota,

The AZ series has a torque limiting feature that you can set as a percentage and when it reaches that torque set it will turn on an output. The output that is turned on when the torque percentage set is reached is the TLC output. The part number would depend on the inertia needed from the application to determine the size of the motor.

Mr.Thota
Posts: 23
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Re: Torque Setting & Limit Feedback

Post by Mr.Thota » Thu Jun 13, 2019 4:23 pm

Thankyou somuch for your reply !! :

Mr.Thota
Posts: 23
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Re: Torque Setting & Limit Feedback

Post by Mr.Thota » Tue Jul 09, 2019 5:40 am

Hi!!
Good Day !!

As we are going to finalize the models Motor: AZM98A0C + Built-In Controller: AZD-CD + Cable: CC030VZR for torque limiting application.
Please advise whether we can get different torque values output (like 0.5 Nm, 1.0 Nm, 1.5 Nm and 2.0 Nm) when reaches setting torque right ??
Please be advise in this regard to proceed further in this matter.

Also please provide us TLC output wiring diagram details along with AZ series manual for our reference.

thanking you.

om_tech_support_KR
Posts: 58
Joined: Thu Jan 11, 2018 3:03 pm

Re: Torque Setting & Limit Feedback

Post by om_tech_support_KR » Tue Jul 09, 2019 11:29 am

Hi Mr. Thota,

You can set the torque limiting as a percentage on the MEXE02 software or with RS485 communication. To match it to the torque value you want to set you would have to reference the speed torque curve and look at the torque needed as a percentage at the specific speed. I will link the speed torque curve below.

azm98ac.jpg
azm98ac.jpg (39.37 KiB) Viewed 736 times

You can reference a sample wiring diagram of the outputs in the manual on page 177 and 179. The TLC output isn't factory set as one of the default outputs but you can use the MEXE02 software or RS485 communication to set it as one of the outputs.

https://www.orientalmotor.com/products/ ... 262-6E.pdf

Mr.Thota
Posts: 23
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Re: Torque Setting & Limit Feedback

Post by Mr.Thota » Tue Jul 09, 2019 9:51 pm

Hi,
Good Day !!
Thankyou verymuch for valued information provided by you.
Thankyou verymuch for your support !!

Post Reply