CVK-SC Series Stepper Motor

Discuss Stepper motors, Drivers, Controllers, GUI's and related Accessories here.
Post Reply
Mr.Thota
Posts: 23
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

CVK-SC Series Stepper Motor

Post by Mr.Thota » Fri Jun 21, 2019 12:25 am

Hi !!

As we would like to use this combination stepper motor unit ( Motor: PKP569FN24A2 + Contorl: CVD524B-KSC + Cable: LC2B06E + I/O Cable: LCS04SD5), which can be run by continuous duty cycle operation by giving ON/OFF switching input voltage (24VDC) ??

Hope this is not pulse input type right ?? and do not required PLC & pulse signalrs right ??

Requested to please clarify the same to proceed further.

om_tech_support_KR
Posts: 58
Joined: Thu Jan 11, 2018 3:03 pm

Re: CVK-SC Series Stepper Motor

Post by om_tech_support_KR » Fri Jun 21, 2019 12:28 pm

Hi Mr.Thota,

You are correct that driver would be the speed control driver where you can program 2 speeds a high speed and a low speed with the dials and switches on the driver. You would then choose the high or low speed with the I/O and the direction with the FWD or RVS input. The inputs can accept a 5-24 VDC signal if you use more than 5 VDC you will have to add resistors to limit the current. I will link the manual below for your reference. Also the correct motor cable would be LC5N06E the LC2B06E cable would be for 2 phase motors.

https://www.orientalmotor.com/products/ ... 60346E.pdf

Mr.Thota
Posts: 23
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Re: CVK-SC Series Stepper Motor

Post by Mr.Thota » Mon Jun 24, 2019 12:24 am

Thankyou somuch for your details !!

Post Reply