BMU Series Clarifications

Discuss Brushless DC Motor Speed Control Systems or AC Motor Speed Control systems and related Accessories here.
Post Reply
Mr.Thota
Posts: 14
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

BMU Series Clarifications

Post by Mr.Thota » Sat Jul 13, 2019 4:43 am

Hi !!
Good Day !!

We are planning to use BMU Series for one of Conveyor Application, wherein we required to control Forward & REverse directions through our PLC, ineed we required the clarifications for the follwing:

1. Please provide us MCB rating (Circuit Breaking) for BMU 30 Watts & 120 Watts ??
2. Regarding the I/O signals, we want to use forward (X0) & reverse (X1) terminals only, whether it is mandatory to use terminal X2 also ??
3. What is the X2 terminal ?? which signal is used to select the operation data ?? without using this how it would be ??

REquested to please clarify the same.

thnaking you and REgards,

Mr.Thota
Posts: 14
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Re: BMU Series Clarifications

Post by Mr.Thota » Sun Jul 14, 2019 12:51 am

Hi !!
Good Day !!

Requested to please ignore our post on 13th July, and requested to please consider below mail as on priority and orgnize the reply at the earliest.

We are planning to use BMU Series for one of Conveyor Application, wherein we required to control Forward & Reverse directions through our PLC, indeed we required the clarifications for the following:

1. Please provide us MCB rating (Circuit Breaking) for BMU 30 Watts & 120 Watts (BLM460S-30B + BMUD60-C2 and BLM5120HPK-5H30S + BMUD120-C2) ??
2. Regarding the I/O signals, we want to use forward (X0) & reverse (X1) terminals only, whether it is mandatory to use terminal X2 also ??
3. What is the X2 terminal ?? which signal is used to select the operation data ?? without using this how it would be ??
4. What is the use of X2 terminal and whether shall we use without X2 Also. We are plan to use only X0 , X1 .
5. We may will take the output in future ( Whether is this like Digital output) ??
6. What is the Current Consumption at 100 rpm 3.5 N-m for both models (We know 60 Watts Rated Current is 1 Amps,230 V Ac ; 120 watts Rated Current is 2 Amps , 230 V Ac ) as above said models.

Requested to please clarify the above, as we need to be take further decision in this regard.

Thanking you and Best Regards,

Post Reply