CVK Series TIM & Alarm Output

Discuss Stepper motors, Drivers, Controllers, GUI's and related Accessories here.
Post Reply
Mr.Thota
Posts: 27
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

CVK Series TIM & Alarm Output

Post by Mr.Thota » Sat Aug 03, 2019 4:41 am

Hi !!

As we are working with PKP268D28B2 + CVD228BR-K + LC2B06E combination, wherein the TIM ouput which we are getting is voltage 0.2 ~ 0.5 V max.
Which we would like to interface to our PLC for measuring values, but our PLC min reading voltage requirement is 20~24V DC.

Hence requested to please let us know how to boost up output saturated voltage 0.5 V to 24 V DC ?? (from TIM & Alarm)

Also please suggest us alternate option, that any other output which gives 24 V DC ??

Thanking you and Best Regards,

om_tech_support_KR
Posts: 67
Joined: Thu Jan 11, 2018 3:03 pm

Re: CVK Series TIM & Alarm Output

Post by om_tech_support_KR » Tue Aug 06, 2019 11:23 am

Hi Mr.Thota,

For the CVD228BR-K driver since they are open-collector type outputs you have to supply the 24 VDC voltage to the output to read that voltage when outputs are on. Reference page 8 of the link below for sample wiring diagram. You will have to use resistors to limit the current to less than 10 mA.

https://www.orientalmotor.com/products/ ... 128-8E.pdf

Mr.Thota
Posts: 27
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Re: CVK Series TIM & Alarm Output

Post by Mr.Thota » Sat Aug 10, 2019 5:05 am

Hi !!

Thankyou verymuch for your details, we are trying but unable to get TIM output 24V DC to read my PLC through this.
A bit confusion about wiring, we need to be provide 24V DC to pin no. 11 & 12 (or) 9 & 10 ??
could you able to discribe the pin details exactly please !!
please do the favourable.

thanks and regards,

om_tech_support_KR
Posts: 67
Joined: Thu Jan 11, 2018 3:03 pm

Re: CVK Series TIM & Alarm Output

Post by om_tech_support_KR » Tue Aug 13, 2019 6:34 am

Hi Mr.Thota,

From the wiring diagram the 24 VDC would go to pins 9 and 11. The pins 10 and 12 would go to 0 VDC. When using 24 VDC use a resistor 2.4 Kohm or larger to keep current at 10 mA or less.

Mr.Thota
Posts: 27
Joined: Tue Oct 02, 2018 9:45 pm
Location: New Jersey

Re: CVK Series TIM & Alarm Output

Post by Mr.Thota » Wed Aug 14, 2019 12:11 am

Thankyou verymuch for your kind support..

Post Reply