Immediate Motion Creator for CM, Save System Config

Discuss Linear or Rotary Actuators, GUI's and related Accessories here.
michael_damm
Posts: 2
Joined: Thu Feb 02, 2012 7:45 am

Immediate Motion Creator for CM, Save System Config

Postby michael_damm » Thu Feb 02, 2012 7:55 am

I wish do save the system configuration of a CM10 to a file, so that I can tranfer them to an other CM10.
I can't find this function in the Immediate Motion Creator.

with regards from germany
Michael Damm

User avatar
techsupport
Posts: 11
Joined: Tue Jan 05, 2010 8:59 am

Re: Immediate Motion Creator for CM, Save System Config

Postby techsupport » Thu Feb 02, 2012 8:14 am

Hi Michael,

In order to save all of the parameters from the SCX10 to a file, you will need to go to the program editor tab. You need to look under the Duplicate Heading on the right side of the screen. In the "All Data" box, click on SCX10 => PC. This will send all of the system configurations to a text file which you can then save on your PC. To upload this date, simply click on the PC => SCX10 and send the text file with the system parameters you saved previously. After the download is complete, save and reset the unit. I hope this helps.

Sincerely,

TechSupport

michael_damm
Posts: 2
Joined: Thu Feb 02, 2012 7:45 am

Re: Immediate Motion Creator for CM, Save System Config

Postby michael_damm » Thu Feb 02, 2012 9:33 am

Thanks thats helps.

Sincerely,
Mike


Return to “Linear and Rotary Actuators and Controls”

Who is online

Users browsing this forum: No registered users and 0 guests