Seeking help for replacement motor.

dwlewis1125
Posts: 1
Joined: Wed Oct 01, 2014 5:41 pm

Seeking help for replacement motor.

Postby dwlewis1125 » Wed Oct 01, 2014 5:44 pm

The motor I am looking to replace is a 5IK40RA-C2. The #2 in the part number on the label is half the size as the other numbers/letters. Any help with this would be greatly appreciated.

User avatar
om_tech_support_JT
Posts: 1058
Joined: Fri Mar 12, 2010 2:59 pm
Location: Torrance, CA
Contact:

Re: Seeking help for replacement motor.

Postby om_tech_support_JT » Thu Oct 09, 2014 2:22 pm

Hi dwlewis1125,

The 5IK40RA-C2 model refers to a 40W induction motor rated for single-phase 200VAC (Japanese standard product). The suggested replacement would be 5IK40RA-CW2J (200VAC; Japanese standard) or 5IK40RA-CW2E (220VAC; US standard). If you're still using single-phase 200VAC, then I would suggest replacing with 5IK40RA-CW2J.


Return to “AC Motors”

Who is online

Users browsing this forum: No registered users and 0 guests